Question
Need RTC Configuration in wakeup counter mode with 1sec wake up time and LSE as Clock source.
Hi Team,
Need the RTC Code base with LSE as clock source in wake-up counter mode and needs to get the interrupt at every 1sec rate.
We have some queries regarding the LSI Clock source which is in example project.
- If we use the LSI as Clock, calibration is required continuously or at a certain frequency only it is required, if required at what frequency we need to calibrate.
- If we use the LSE as Clock source also calibration is required or not.
- Can we give the source code for the RTC in Wakeup counter mode with LSE as Clock source with all register settings and how to calculate the wake-up counter value with all clock pre scalar register settings values.
- Reason is as compared to LSI clock LSE is more accurate and calibration is not required in run time, please correct me my assumption is wrong.
Regards,
Srinivas.V