Skip to main content
rick_thompson
Associate
October 16, 2007
Question

Need more ram

  • October 16, 2007
  • 2 replies
  • 655 views
Posted on October 16, 2007 at 15:24

Need more ram

    This topic has been closed for replies.

    2 replies

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    you can use serial SPI SRAM , but they only go up to 32Kbytes, but they are cheap (30 cents/10K) so you can gang four together, but this is very slow, how fast does it have to be?

    or use parallel SRAM using I/O ports to simulate the an external bus (easy to do, speed is much better then serial, but not as fast as internal), using this method you can easily get 128K and much more if needed, but you need a lot of spare ports

    Finding 128K SRAM internal is hard, only a few ARM's support that amount of memory and you tend to get alot of junk you don't want and you won't be able to expand, so I don't like that option

    rick_thompson
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    What is a simple way to add about 128K bytes of ram? It can be volatile. Should I be considering some other ARM type product?

    Thanks