Skip to main content
BAl K.1
Associate III
January 24, 2023
Question

Need help with PN532 via HSU to STM32F405

  • January 24, 2023
  • 1 reply
  • 980 views

I need help with to access the pn532 nfc to stm32f405 via HSU. i have looked many references but some of them are in i2c. And i need help with HSU way, please help anyone

This topic has been closed for replies.

1 reply

Foued_KH
ST Employee
February 10, 2023

Hello @BAl K.1​ ,

The PN532 supports the following host interfaces:

• SPI

• I2C

• High Speed UART (HSU)

I2C communication :

  • I2C Standard mode (100 kHz SCLK) and Fast mode (400 kHz SCLK) are supported
  • for more information ( 8.3.2.1 I2C functional description Datasheet)

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.