Skip to main content
Robert Harrison
Associate
May 10, 2018 7:28 AM UTC
Question

Need help with CRC unit

Posted on May 10, 2018 at 09:28

STM32L452C

My code:

__HAL_RCC_CRC_CLK_ENABLE();

CRC->POL = (uint32_t) 0x1021;//CRC-16-CCITT

CRC->INIT = (uint32_t) 0xFFFF;

CRC->CR = (uint32_t) 0x09;//REV_OUT = 0, REV_IN = 00, POLYSIZE = 01, RESET = 1

CRC->DR = '1';

CRC->DR = '2';

CRC->DR = '3';

CRC->DR = '4';

The correct result for this CRC is 0x5349 but when I read the DR I get 0xb23b

I have tried all combinations of input and output bit reversal, doesn't work.

    This topic has been closed for replies.

    4 replies

    Nesrine M_O
    Associate
    May 10, 2018 8:18 AM UTC
    Posted on May 10, 2018 at 10:18

    Hi

    robert.015

    ,

    I recommend you to have a look to CRC examples under the STM32L4 firmware package, it may helpful to start your own project:STM32Cube_FW_L4_V1.0\Projects\NUCLEO-L452RE\Examples\CRC

    -Nesrine-

    Robert Harrison
    Associate
    May 10, 2018 10:59 AM UTC
    Posted on May 10, 2018 at 10:59

    Thanks. I just realised that the cubeMX utility doesn't copy all the HAL drivers to your project dir. I was missing 'stm32l4xx_hal_crc.c' etc.

    Nesrine M_O
    Associate
    May 16, 2018 5:48 PM UTC
    Posted on May 16, 2018 at 17:48

    Could you please  precise the MX version are you using?

    if your are using an older version please use the latest one and tell us if the issue still again

    Tesla DeLorean
    Guru
    May 16, 2018 3:55 PM UTC
    Posted on May 16, 2018 at 17:55

    DR is a 32-bit wide register, you need to write bytes 8-bit wide, thusly...

    *((volatile uint8_t *)&CRC->DR) = '1';

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..