Question
Need Help setting up STM32Discovery
Posted on April 09, 2011 at 02:22
Hello there
I'm really new to this :) i was wondering if someone can help me to set up my STM32 VL Discivery. so far I have done the following; I'm using Vista home premium I installed Eclipse galileo / Helios and ST link ST-LINK_gdbserverCodesourcery Lite EABI toolchain
And i have installed the follwoing Plugins for eclipseGNU Arm Development Tools
Zylin Embedded CDT
so when try to debug a code I'm getting the following two errors ''Remote communication error. Target disconnected.: No error.load
You can't do that when your target is `exec'
break main''
sometimes i get this
''localhost:61234: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond.
load
You can't do that when your target is `exec'
break main'' if someone can help to fix this :) thanks Harshi