Skip to main content
Ubus99
Associate III
October 12, 2020
Question

Need help setting up DMA on STM32F1 & F4

  • October 12, 2020
  • 6 replies
  • 1557 views

Hi, I am trying to set up an input capture with DMA on a F1 and a F4 chip.

The documentation is confusing, and most tutorials don't work for my specific scenario. For a start, when setting up DMA using cubeMX, I can't configure source, destination and data length.

Reading the Documentation I should use HAL_DMA_START(); and put those values in there, but when called, it just tells me that the DMA controller is busy. I can't find any resources about what that means, what do I need to change?

And getting the hdma is tedious as well. I got it working using

htim1.hdma[TIM_DMA_ID_CC1]

But there got to be a better way.

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
October 12, 2020

> Hi, I am trying to set up an input capture with DMA on a F1 and a F4 chip.

What exactly is the problem?

Describe, what' you've done, in terms of TIM and DMA registers content, one chip at a time.

JW

Ubus99
Ubus99Author
Associate III
October 12, 2020

I did most of the configuration in MX:

TIM1:

  • Channel 1 input capture on PA8
  • pull-down
  • DMA2 Stream 1

DMA:

  • Same as above,
  • Circular
  • low priority
  • Half Word.

My Main.c:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_ch1;
 
UART_HandleTypeDef huart2;
 
/* USER CODE BEGIN PV */
uint8_t test[6];
uint16_t timer;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM1_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void) {
	/* USER CODE BEGIN 1 */
 
	/* USER CODE END 1 */
 
	/* MCU Configuration--------------------------------------------------------*/
 
	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();
 
	/* USER CODE BEGIN Init */
 
	/* USER CODE END Init */
 
	/* Configure the system clock */
	SystemClock_Config();
 
	/* USER CODE BEGIN SysInit */
 
	/* USER CODE END SysInit */
 
	/* Initialize all configured peripherals */
	MX_GPIO_Init();
	MX_DMA_Init();
	MX_USART2_UART_Init();
	MX_TIM1_Init();
	/* USER CODE BEGIN 2 */
 
	HAL_TIM_Base_Start(&htim1);
	HAL_DMA_Start(htim1.hdma[TIM_DMA_ID_CC1], (uint32_t) &TIM1->CCR1,
			(uint32_t) &test, 0x06); //god i hope this works
	/* USER CODE END 2 */
 
	/* Infinite loop */
	/* USER CODE BEGIN WHILE */
	while (1) {
		/* USER CODE END WHILE */
 
		/* USER CODE BEGIN 3 */
	}
	/* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void) {
	RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
	RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
 
	/** Configure the main internal regulator output voltage
	 */
	__HAL_RCC_PWR_CLK_ENABLE();
	__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
	/** Initializes the RCC Oscillators according to the specified parameters
	 * in the RCC_OscInitTypeDef structure.
	 */
	RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
	RCC_OscInitStruct.HSIState = RCC_HSI_ON;
	RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
	RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
	RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
	RCC_OscInitStruct.PLL.PLLM = 16;
	RCC_OscInitStruct.PLL.PLLN = 336;
	RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
	RCC_OscInitStruct.PLL.PLLQ = 7;
	if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
		Error_Handler();
	}
	/** Initializes the CPU, AHB and APB buses clocks
	 */
	RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
			| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
	RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
	RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
	RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
	RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
	if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) {
		Error_Handler();
	}
}
 
/**
 * @brief TIM1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM1_Init(void) {
 
	/* USER CODE BEGIN TIM1_Init 0 */
 
	/* USER CODE END TIM1_Init 0 */
 
	TIM_ClockConfigTypeDef sClockSourceConfig = { 0 };
	TIM_MasterConfigTypeDef sMasterConfig = { 0 };
	TIM_IC_InitTypeDef sConfigIC = { 0 };
 
	/* USER CODE BEGIN TIM1_Init 1 */
 
	/* USER CODE END TIM1_Init 1 */
	htim1.Instance = TIM1;
	htim1.Init.Prescaler = 4;
	htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
	htim1.Init.Period = 65535;
	htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
	htim1.Init.RepetitionCounter = 0;
	htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
	if (HAL_TIM_Base_Init(&htim1) != HAL_OK) {
		Error_Handler();
	}
	sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
	if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) {
		Error_Handler();
	}
	if (HAL_TIM_IC_Init(&htim1) != HAL_OK) {
		Error_Handler();
	}
	sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
	sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
	if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig)
			!= HAL_OK) {
		Error_Handler();
	}
	sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
	sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
	sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
	sConfigIC.ICFilter = 0;
	if (HAL_TIM_IC_ConfigChannel(&htim1, &sConfigIC, TIM_CHANNEL_1) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN TIM1_Init 2 */
 
	/* USER CODE END TIM1_Init 2 */
 
}
 
/**
 * @brief USART2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_USART2_UART_Init(void) {
 
	/* USER CODE BEGIN USART2_Init 0 */
 
	/* USER CODE END USART2_Init 0 */
 
	/* USER CODE BEGIN USART2_Init 1 */
 
	/* USER CODE END USART2_Init 1 */
	huart2.Instance = USART2;
	huart2.Init.BaudRate = 115200;
	huart2.Init.WordLength = UART_WORDLENGTH_8B;
	huart2.Init.StopBits = UART_STOPBITS_1;
	huart2.Init.Parity = UART_PARITY_NONE;
	huart2.Init.Mode = UART_MODE_TX_RX;
	huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
	huart2.Init.OverSampling = UART_OVERSAMPLING_16;
	if (HAL_UART_Init(&huart2) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN USART2_Init 2 */
 
	/* USER CODE END USART2_Init 2 */
 
}
 
/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) {
 
	/* DMA controller clock enable */
	__HAL_RCC_DMA2_CLK_ENABLE();
 
	/* DMA interrupt init */
	/* DMA2_Stream1_IRQn interrupt configuration */
	HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void) {
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };
 
	/* GPIO Ports Clock Enable */
	__HAL_RCC_GPIOC_CLK_ENABLE();
	__HAL_RCC_GPIOH_CLK_ENABLE();
	__HAL_RCC_GPIOA_CLK_ENABLE();
	__HAL_RCC_GPIOB_CLK_ENABLE();
 
	/*Configure GPIO pin Output Level */
	HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
 
	/*Configure GPIO pin : B1_Pin */
	GPIO_InitStruct.Pin = B1_Pin;
	GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
 
	/*Configure GPIO pin : LD2_Pin */
	GPIO_InitStruct.Pin = LD2_Pin;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void) {
	/* USER CODE BEGIN Error_Handler_Debug */
	/* User can add his own implementation to report the HAL error return state */
 
	/* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

The Code runs, but the DMA doesn't, i suspect its because the HAL_DMA_START function fails, breakpoints show it's because the DMA is busy

--------------------------------------------------------

I am using

 htim1.hdma[TIM_DMA_ID_CC1]

because when writing for F1, the hdma is declared in the TIM.c file and isn't in the scope of main.c, I could change that, but am unsure if this is the intended way of doing it.

MM..1
Super User
October 12, 2020

Try swap tim base start with dma start

Ubus99
Ubus99Author
Associate III
October 12, 2020

did that before, this is the second version. Neither work.

waclawek.jan
Super User
October 12, 2020

This is which STM32 exactly? Let's discuss only one of them for now.

Did you verify that the capture works?

Read out and check/post the TIM, DMA and relevant GPIO registers' content.

I don't Cube/CubeMX.

JW

Ubus99
Ubus99Author
Associate III
October 13, 2020

Hi Waclawek, I am currently working on a nucleoF401RE for development purposes, but in production we use F1RCTs on custom boards (I know, I know...)

I went through the code step by step and checked against the documentation, and I found that I used the wrong start function.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_ch1;
 
UART_HandleTypeDef huart2;
 
/* USER CODE BEGIN PV */
uint32_t test[6];
uint32_t timer;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM1_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void) {
	/* USER CODE BEGIN 1 */
 
	/* USER CODE END 1 */
 
	/* MCU Configuration--------------------------------------------------------*/
 
	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();
 
	/* USER CODE BEGIN Init */
 
	/* USER CODE END Init */
 
	/* Configure the system clock */
	SystemClock_Config();
 
	/* USER CODE BEGIN SysInit */
 
	/* USER CODE END SysInit */
 
	/* Initialize all configured peripherals */
	MX_GPIO_Init();
	MX_DMA_Init();
	MX_USART2_UART_Init();
	MX_TIM1_Init();
	/* USER CODE BEGIN 2 */
 
	//HAL_TIM_Base_Start_DMA(&htim1, test, 6);
	HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, test, sizeof test);
 
	/* USER CODE END 2 */
 
	/* Infinite loop */
	/* USER CODE BEGIN WHILE */
	while (1) {
		timer = __HAL_TIM_GET_COUNTER(&htim1);
		/* USER CODE END WHILE */
 
		/* USER CODE BEGIN 3 */
	}
	/* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void) {
	RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
	RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
 
	/** Configure the main internal regulator output voltage
	 */
	__HAL_RCC_PWR_CLK_ENABLE();
	__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
	/** Initializes the RCC Oscillators according to the specified parameters
	 * in the RCC_OscInitTypeDef structure.
	 */
	RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
	RCC_OscInitStruct.HSIState = RCC_HSI_ON;
	RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
	RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
	RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
	RCC_OscInitStruct.PLL.PLLM = 16;
	RCC_OscInitStruct.PLL.PLLN = 336;
	RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
	RCC_OscInitStruct.PLL.PLLQ = 7;
	if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
		Error_Handler();
	}
	/** Initializes the CPU, AHB and APB buses clocks
	 */
	RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
			| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
	RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
	RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
	RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
	RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
	if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) {
		Error_Handler();
	}
}
 
/**
 * @brief TIM1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM1_Init(void) {
 
	/* USER CODE BEGIN TIM1_Init 0 */
 
	/* USER CODE END TIM1_Init 0 */
 
	TIM_ClockConfigTypeDef sClockSourceConfig = { 0 };
	TIM_MasterConfigTypeDef sMasterConfig = { 0 };
	TIM_IC_InitTypeDef sConfigIC = { 0 };
 
	/* USER CODE BEGIN TIM1_Init 1 */
 
	/* USER CODE END TIM1_Init 1 */
	htim1.Instance = TIM1;
	htim1.Init.Prescaler = 4;
	htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
	htim1.Init.Period = 65535;
	htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
	htim1.Init.RepetitionCounter = 0;
	htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
	if (HAL_TIM_Base_Init(&htim1) != HAL_OK) {
		Error_Handler();
	}
	sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
	if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) {
		Error_Handler();
	}
	if (HAL_TIM_IC_Init(&htim1) != HAL_OK) {
		Error_Handler();
	}
	sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
	sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
	if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig)
			!= HAL_OK) {
		Error_Handler();
	}
	sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
	sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
	sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
	sConfigIC.ICFilter = 0;
	if (HAL_TIM_IC_ConfigChannel(&htim1, &sConfigIC, TIM_CHANNEL_1) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN TIM1_Init 2 */
 
	/* USER CODE END TIM1_Init 2 */
 
}
 
/**
 * @brief USART2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_USART2_UART_Init(void) {
 
	/* USER CODE BEGIN USART2_Init 0 */
 
	/* USER CODE END USART2_Init 0 */
 
	/* USER CODE BEGIN USART2_Init 1 */
 
	/* USER CODE END USART2_Init 1 */
	huart2.Instance = USART2;
	huart2.Init.BaudRate = 115200;
	huart2.Init.WordLength = UART_WORDLENGTH_8B;
	huart2.Init.StopBits = UART_STOPBITS_1;
	huart2.Init.Parity = UART_PARITY_NONE;
	huart2.Init.Mode = UART_MODE_TX_RX;
	huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
	huart2.Init.OverSampling = UART_OVERSAMPLING_16;
	if (HAL_UART_Init(&huart2) != HAL_OK) {
		Error_Handler();
	}
	/* USER CODE BEGIN USART2_Init 2 */
 
	/* USER CODE END USART2_Init 2 */
 
}
 
/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) {
 
	/* DMA controller clock enable */
	__HAL_RCC_DMA2_CLK_ENABLE();
 
	/* DMA interrupt init */
	/* DMA2_Stream1_IRQn interrupt configuration */
	HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void) {
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };
 
	/* GPIO Ports Clock Enable */
	__HAL_RCC_GPIOC_CLK_ENABLE();
	__HAL_RCC_GPIOH_CLK_ENABLE();
	__HAL_RCC_GPIOA_CLK_ENABLE();
	__HAL_RCC_GPIOB_CLK_ENABLE();
 
	/*Configure GPIO pin Output Level */
	HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
 
	/*Configure GPIO pin : B1_Pin */
	GPIO_InitStruct.Pin = B1_Pin;
	GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
 
	/*Configure GPIO pin : LD2_Pin */
	GPIO_InitStruct.Pin = LD2_Pin;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void) {
	/* USER CODE BEGIN Error_Handler_Debug */
	/* User can add his own implementation to report the HAL error return state */
 
	/* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Now it starts the timer, captures the signal and transfers it.

Thing is, the data that I get out is weird, probably because the input capture is faster than I can remove the signal, then again, I told it only to capture on a rising edge.

My circular buffer is getting overwritten completely when connecting the debug-wires.