My results when examining interrupt latency of a STM32F439
Hello,
I just started with a Nucleo F439ZI and did some tests to examine interrupt latency and code execution times. Here are my results and a number of questions:
I set the system to the maximum speed using CubeMX, so I have HCLK and FCLK = 180MHz, APB1/2 Timer clk = 90MHz, APB1/2 periph clk = 45MHz.
I generate a 10 kHz PWM signal with TIM2 and output it on channel 1 on pin PA5. Also I made this event trigger an interrupt and the isr is this, outputting a short puls on PA6:
void TIM2_IRQHandler (void)
{
//SetPortBit (port_Testpins, pin_Timer2_isr);
GPIOA->BSRR=1U<<(6);
__NOP ();
//ClearPortBit (port_Testpins, pin_Timer2_isr);
GPIOA->BSRR=(1U<<16)<<(6);
ClearBitMask (TIM2->SR, TIM_SR_CC1IF);
}180MHz is 5,5 nsec per instruction so I first expected the given 12 cycles (eg here http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/ka16366.html) to result in a time between the falling edge of the PWM signal and the rising edge on PA6 of about 70 nsec. But I got between 194 and 216 nsec, jittering.
Then I found, that CubeMX also set my system to 5 wait states and looking into ref manual I found that running the controller at 30 MHz needs no wait states ie 1 CPU cycle per flash read which is 33 nsec. Running it at 180 MHz needs 5 wait states, so 6 CPU cycles per flash read which is also 33 nsec.
I also found options instruction prefetch and instruction cache in FLASH->ACR. Enabling both reduces the time to between 144 nsec and 177 nsec.
Strange for my understanding is that commenting out the nop instruction reduces jitter significantly while not decreasing the pulse width.
Changing compiler optimization level from none to speed I get a very short pulse without nop, but the same interrupt latency while with nop I get a latency of 134 nsec without any jitter.
I would appreciate some background information on these behaviours, especially what instruction prefetch and cache are doing and what is their use in case of an isr being loaded.
Then I would like to ask where precisely the higher clock frequency reduces execution speed when the flash read cycles do not benefit from it, I was very surprised to find this.
Is it an option to copy the isr to RAM and execute it there? Will this reduce interrupt latency? Is code running in RAM executing faster than from flash? Where can I find some information about how to do this, isr and normal C-functions. I couldn't find anything detailed.
Thanks a lot for any help and information
Martin