Question
My adc on a STM32F091RC does not work anymore after CubeMX upgrade
Posted on January 29, 2018 at 09:30

Hi. I have a very strange behaviour with adc.
The CubeMX setup is shown below

This is my empty callback
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) {
}And the main
int main(void)
{ HAL_Init();SystemClock_Config();
MX_GPIO_Init();
MX_ADC_Init();HAL_ADC_Start_IT(&hadc);
while (1)
{ HAL_GPIO_WritePin(Led0_GPIO_Port, Led0_Pin, GPIO_PIN_SET); HAL_Delay(100); HAL_GPIO_WritePin(Led0_GPIO_Port, Led0_Pin, GPIO_PIN_RESET); HAL_Delay(100); }}
The program does not work. In order to have my led blinking it working I have to comment out the line
HAL_ADC_Start_IT(&hadc);
What is wrong?