Skip to main content
Associate II
Mar 11, 2024 6:32 PM UTC
Question

Multiplexing I2C on STM32f4 Board

Hi all

I am using 4 sensors on my project. These are comminicated with stm32f4 board via I2C. However there ara 3 I2C channel on stm32f4 board. Is it possible to connect them to same channel via  ı2c multiplexer ? As ı researched, the multiplexer is used with the same sensors. The multiplexer i mentionoed is TCA9548A. 

This topic has been closed for replies.

10 replies

Andrew Neil
Super User
Mar 11, 2024 6:46 PM UTC

@yasinbjk50 wrote:

stm32f4 board  


Which STM32F4 board - an ST board, or your own custom board?

Fundamental to the operation of I2C is the Slave Address - that's what lets you have multiple Slaves on a single I2C bus.

Do your sensors not allow you to select different addresses?

 


@yasinbjk50 wrote:

The multiplexer i mentionoed is TCA9548A. 


So this:

https://www.ti.com/product/TCA9548A

Yes, as its datasheet shows, that is designed to allow a single I2C Master to connect to multiple I2C buses:

AndrewNeil_0-1710182671908.png

AndrewNeil_1-1710182785098.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Mar 13, 2024 10:08 AM UTC

The board ı am using is 32f407vg. However the sensors are different from each other (rtc module, pulse sensor, lux sensor, lcd module). As ı understand, TCA9548A is used for connecting same sensors. Is it appropriate device for my project?

AScha.3
Super User
Mar 11, 2024 6:54 PM UTC
If you feel a post has answered your question, please click on " Best Answer ".
Karl Yamashita
Principal
Mar 11, 2024 9:49 PM UTC

What sensor are you interfacing to? Most I2C devices can be hardwired for a different address. Then in FW, you can read/write to each sensor address independently. Knowing what sensor would clarify this.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate II
Mar 13, 2024 10:13 AM UTC

DS1307 (RTC module), BH1705(Light Sensor), MAX30100 (Pulse Sensor), LCD Sensor. So these are much more than ı have I2C on STM32f407vg

Andrew Neil
Super User
Mar 13, 2024 10:34 AM UTC

@yasinbjk50 wrote:

The board ı am using is 32f407vg. 


That's not a board - that's just a chip.

Is that STM32F407VG chip mounted on an ST board, or a 3rd-party board, or your own custom board?

 


@yasinbjk50 wrote:

However the sensors are different from each other (rtc module, pulse sensor, lux sensor, lcd module)


Then they should all have different I2C Slave Addresses - yes?

 


@yasinbjk50 wrote:

As ı understand, TCA9548A is used for connecting same sensors


Generally, yes - or, at least, devices which all have the same I2C Slave Address.

 


@yasinbjk50 wrote:

 Is it appropriate device for my project?


Probably not: all your sensors should have different I2C Slave Addresses - so you shouldn't need a multiplexer for that.

Unless you have some other specific reason for it?

 


@yasinbjk50 wrote:

DS1307 (RTC module), BH1705(Light Sensor), MAX30100 (Pulse Sensor), LCD Sensor. So these are much more than ı have I2C on STM32f407vg


The datasheets for all these devices will tell you what I2C Slave Address(es) each one has.
(often devices have a choice of 2 or more addresses to minimise the risk of "collisions")

What is an "LCD Sensor"?
LCDs are usually output devices - so not "sensors" ...
:thinking_face:

 


@yasinbjk50 wrote:

 So these are much more than ı have I2C on STM32f407vg


Pardon?

The whole point of a bus is that it can be shared by multiple devices - I2C is a bus.

You can connect multiple devices to an I2C bus - it is the Slave Address which distinguishes them.

Example from Wikipedia:

AndrewNeil_0-1710327488882.png

 

Perhaps you need to read-up on the I2C bus:

https://en.wikipedia.org/wiki/I%C2%B2C

UM10204 2C-bus specification and user manual - this is the definitive specification of the  I2C bus:

https://www.nxp.com/docs/en/user-guide/UM10204.pdf

There are many 3rd-party tutorials; eg,

https://learn.sparkfun.com/tutorials/i2c/all

https://www.i2c-bus.org/

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 13, 2024 2:21 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.