Skip to main content
LMorr.3
Senior
April 10, 2024
Solved

Multiplex 1 output to 12

Hello,

What is the best way to multiplex an output pin to 12 output signals?  I currently have 1 output sourcing 3.3v through a 1k resistor which works well, but need it multiplexed to 12 identical outputs.  I see the STM32F373 has a max rating of 15mA for output pins so looking for advice on the best way to handle this.

Many thanks,

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
April 11, 2024

Where did you see this rating of 15uA (microamps)?

I would expect the rating to be 15mA (milliamps), 1000 times as much.

I think you are misunderstanding the term Multiplex. That is where different signals are shared on the same pin. Perhaps a better term for what I understand you want is fan-out. And where you are driving only CMOS inputs the fan-out is unlimited (subject to speed issues caused by stray capacitance). And this can be improved by Buffering

You might want to consider ESD protection where signals go from one pcb to another, or opto-isolation if they might not share the same Vss.

9 replies

Andrew Neil
Super User
April 10, 2024

I think we need more details of the nature of this output signal, what it has to feed, and what you mean by "multiplexing" here, and what are the constraints, timing requirements, etc ?

A diagram might help ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LMorr.3
LMorr.3Author
Senior
April 10, 2024

Here is more detail:  The main uC can connect up to 12 other uCs.  The main uC can send a 3.3V signal 'trigger' signal to other uCs via an output pin.  Currently, I have the main uC sending successfully to 1 other uC but now need to duplicate ( multiplex ) the signal to all other uCs.  Looking at using TI parts but will need 2 and may be overkill.  

Many thanks,

mƎALLEm
ST Technical Moderator
April 10, 2024
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
April 10, 2024

Need to be more specific.

What do you mean by "an output pin"? Analog output ex: from F3 DAC? 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Danish1
Danish1Best answer
Lead III
April 11, 2024

Where did you see this rating of 15uA (microamps)?

I would expect the rating to be 15mA (milliamps), 1000 times as much.

I think you are misunderstanding the term Multiplex. That is where different signals are shared on the same pin. Perhaps a better term for what I understand you want is fan-out. And where you are driving only CMOS inputs the fan-out is unlimited (subject to speed issues caused by stray capacitance). And this can be improved by Buffering

You might want to consider ESD protection where signals go from one pcb to another, or opto-isolation if they might not share the same Vss.

LMorr.3
LMorr.3Author
Senior
April 11, 2024

You are correct, I meant mA and not uA.  Fan-out is also good term to describe what I was looking for.  Good to know the fan-out for CMOS is unlimited.  I also have another case where I"m planning on using multiple SN74AHCT1G125 parts and will drive them with 1 output pin.  

Andrew Neil
Super User
April 11, 2024

@LMorr.3  It's still unclear what your requirement here is.

As @Danish1 suggests, it's not even clear what you mean by the term "multiplex"

Again, a diagram may help.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LCE
Principal III
April 11, 2024

Check the load again, when driving 12 GPIOs = hi Z inputs of other MCUs, the STM32 output driver should be good enough.

And what Andrew said, what about using more pins?
You could use a complete GPIO-bank to drive the pins in sync.