Skip to main content
JSorl.1
Associate
February 8, 2023
Question

Multiple images

  • February 8, 2023
  • 1 reply
  • 743 views

Regarding STM32G0B1

In a remotely operated AUV I would like to have a mechanism for two or more full code images with the option of rollback.

1) Is it possible to partition main FLASH in two with a selection mechanism and rollback

2) Ist it possible to have two external images (SPI memory, I2C memory, other memory) that can support a selection mechasim and a rollback

3) Other ideas that can support two full images with a selection mechanism and rollback

4) Are there other options, like bank swap in G4 or other?

best regards

/Jon

This topic has been closed for replies.

1 reply

Javier1
Principal
February 13, 2023

What do you mean with rollback?

>>1) Is it possible to partition main FLASH in two with a selection mechanism and rollback

people normally does 3 partitions, 1 bootloader and 2 different "images"

They are not "partituons" you just define your address space you need for each "image".

>>2) Ist it possible to have two external images (SPI memory, I2C memory, other memory) that can support a selection mechasim and a rollback

the bootloader could use SPI or I2C memory

hit me up in https://www.linkedin.com/in/javiermuñoz/