Skip to main content
Broman3100
Associate III
May 19, 2022 12:52 PM UTC
Solved

Multiple choices for microsecond delay, which one's better?

Hello, First time using the forum so apologies if I mess something up...

Long story short I wanna get a microsecond delay, I know 2 ways of doing it:

1) I can start a timer with default cube values and use a function like:

void delay (uint16_t delay) 
{
	__HAL_TIM_SET_COUNTER(&htim1, 0);
	while( __HAL_TIM_GET_COUNTER(&htim1) < delay);
}

to get the desired delay, or

2) I can start timer, set its prescaler value to specific frequency with interrupt turned on, drop it down to 1khz/mhz for easier calculations and in timer callback function have some variable increase by 1, then use it in different function as time measurement, something similar to this:

uint8_t counter;
 
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
	counter++;
}
 
void main() {
while(){
 if(counter==20){
 // do smth
 counter=0;
 }
 }
}

I have used both of these methods previously and know one is running in blocking mode, other in non-blocking mode. So that got me wondering, what other differences do they have, if blocking mode isn't an issue which one is more preferable to use, takes up less space, is more efficient and accurate? And is there another method even better than these two I can use?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 19, 2022 1:33 PM UTC

The difference in time. ie dt = (TimeB - TimeA)

void delay (uint16_t delay) 
{
 uint16_t start = __HAL_TIM_GET_COUNTER(&htim1);
 while((__HAL_TIM_GET_COUNTER(&htim1) - start) < delay);
}

This can be called from a 100 threads and will behaves more consistently than you resetting it to zero and thresholding against the up-count from there.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

5 replies

Tesla DeLorean
Guru
May 19, 2022 1:10 PM UTC

Having it delta a free-running counter would be more thread/interrupt safe.

Also works for time-outs.

Would avoid interrupting at high speed, and having software counts.

If using a timer with interrupts, have a list of events you are managing, so you aren't creating dozens of different methods for what is a single time-line problem.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Broman3100
Associate III
May 19, 2022 1:17 PM UTC

Thank you for your response;

An odd follow-up question, "Having it delta" - is this (delta) a term I'm not familiar with or a typo?

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 19, 2022 1:33 PM UTC

The difference in time. ie dt = (TimeB - TimeA)

void delay (uint16_t delay) 
{
 uint16_t start = __HAL_TIM_GET_COUNTER(&htim1);
 while((__HAL_TIM_GET_COUNTER(&htim1) - start) < delay);
}

This can be called from a 100 threads and will behaves more consistently than you resetting it to zero and thresholding against the up-count from there.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..