Multiple channels input capture at the same time
Hello, I'd like to know if there is possibility to use all input capture channels at the same time?
For starting timer i use function wich enable only 1 channel:
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, &restWave[0], 1);
I'd like to use something like this (but obviously it doesn't work)
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_ALL, restWave, 4);
And it doesn't work as well:
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, &restWave[0], 1);
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_2, &restWave[1], 1);
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_3, &restWave[2], 1);
HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_4, &restWave[3], 1);