Multiple CAN problems
See also my post How to stop HAL_CAN_ErrorCallback
Something else now. On every CAN receive IRQ the HAL_CAN_TxCpltCallback triggers and nothing has been send. It is because the HAL_CAN_IRQHandler is called by the receive of a CAN message and
__HAL_CAN_TRANSMIT_STATUS(hcan, CAN_TXMAILBOX_0))
__HAL_CAN_TRANSMIT_STATUS(hcan, CAN_TXMAILBOX_1))
Are always true. So the Tx Complete IRQ is also triggered when the Rx triggers. Bug??
The HAL_CAN_RxCpltCallback works well (unlike the UART RX IRQ) after weeks of testing however sometimes the HAL_CAN_Transmit_IT does not tx anymore. So i printed the flags. In case of error i have the CAN_FLAG_EWG and
CAN_FLAG_EPV when it does work i also have this flags after some time. When disconnect the CAN connector there is no BOF as i should aspect.Can ST provide an example of a stable CAN rx and tx routine that keeps working even if the cable has been disconnected.