Skip to main content
Visitor II
Oct 13, 2025 12:01 PM UTC
Question

MT35XU02GCBA2G12-0AUT compatibility with STM32N6 XSPI?

Hi everyone,
Has anyone interfaced the Micron MT35XU02GCBA2G12-0AUT (2 Gbit xccela Flash) with the STM32N6 XSPI controller?

I  would like to know if it works with the existing Macronix presets or needs custom XSPI settings.
Any working example or experience would help.

Thanks!

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
Oct 13, 2025 1:09 PM UTC

Hello @GBA ;

 

Could you please share the memory datasheet?

To check whether a device is supported by the XSPI interface, you need to refer to memory datasheet and the STM32N6 reference manual and precisely the command format and order.

The command format and order shared in the device datasheet must be aligned with the command format and order mentioned in the STM32 reference. 

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.