Skip to main content
GreenGuy
Senior III
May 8, 2018
Question

MPU regions and DMA

  • May 8, 2018
  • 0 replies
  • 573 views
Posted on May 08, 2018 at 23:43

I am confused over the inability to successfully setup an MPU region for the area that the DMA is using.  I am trying to get around having to use Clean and Invalidate Cache like so to guaranty the data is passed correctly:

    SCB_CleanDCache_by_Addr((uint32_t *)EclFrame, ((BytesToSend+31)/32)*32); //works

    result = HAL_UART_Transmit_DMA(&UartHandle, (uint8_t *) EclFrame, BytesToSend);

and:

    result = HAL_UART_Receive_DMA(&UartHandle, (uint8_t *)EclFrame, BufferSize);

    SCB_InvalidateDCache_by_Addr((uint32_t *)EclFrame, ((BufferSize+31)/32)*32); // works

I have tried to setup a region for RAM_D1 like so:

  MPU_InitStruct.Enable = MPU_REGION_ENABLE;

  MPU_InitStruct.BaseAddress = 0x24000000;

  MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;

  MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;

  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

  MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;

  MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; //also tried NOT

  MPU_InitStruct.Number = MPU_REGION_NUMBER4;

  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;

  MPU_InitStruct.SubRegionDisable = 0x00;

  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);

with the result being that the transmit sends the wrong data.  I am not sure about receive since this is used in a command-response sequence hence sending the wrong data out means no data back.  There are three other memory regions setup and they are working fine so I do not get why this region should have a problem.

    This topic has been closed for replies.