Skip to main content
Senior
Feb 29, 2024 11:12 AM UTC
Question

More than one DSMPS on one MCU

I have developed a custom controller that uses the STM32G474RE to regulate the output voltage of two power supplies.

I am now developing the code to implement a peak-current mode controller for each of the two power supplies.  Is there a way that I can use the one FMAC to implement the required filtering for both power supplies?

If not, I suppose that I can use PID control on one of the two power supplies.

Any suggestions would be welcome...

Thank you,

David

 

This topic has been closed for replies.