MODBUS ERROR-RS485 Converter_ Reg
Hi,
I am having data transfer problem with Modbus only when I use a specific RS485 Converter .I am using STM32H750VB as my main IC for a fuel dispenser project. I am having a problem with my MODBUS based on the RS485 converter.
i)If i am using the RS485 converter which consists of MAX 13487E, I don't have any problem with MODBUS(no error).
ii)But if I use an RS485 converter with MAX485 IC then I am having CRC error (the data received is correct but the value of CRC Changes) while receiving the response from my IC.
The error code is :0xbfff006b framing error occurred in Modbus ..1073807253 at VISA Serial Read...
Can anyone suggest how to get the correct output in Modbus in both the cases.
Note:
i)I have checked the output with three Software's : Simply mod bus master , Modbus poll and Modscan64.
ii)The baud rates are correct(9600)
iii)A and B of RS485 are connected correctly
iv)RTU Mode is used with 8 databits,1 stop bit and No parity bit
v)The address for request and response are correct.