Skip to main content
TwelveSquared
Associate III
August 27, 2020
Question

Mistake in STM32G4xx Reference Manual (RM0440)?

The STM32G4xx Reference Manual (RM0440) Rev 4, Figure 2, "Memory Map" on Page 81 says Option Bytes 1 is from 0x1fff7800 to 0x1fff7810 (16 option bytes), Option Bytes 2 is from 0x1ffff800 to 0x1ffff810 (16 option bytes).

However:

Table 7 on page 94 says: Option Bytes 1 is from 0x1fff7800 to 0x1fff782f (48 option bytes) and Option Bytes 2 is from 0x1ffff800 to 0x1ffff82f (48 option bytes).

Is this discrepancy an error?

If not an error, please help me understand!!

Thanks kindly,

This topic has been closed for replies.

2 replies

ST Technical Moderator
August 28, 2020

Hello @TwelveSquared​ ,

You are right. I raised your feedback internally to correct adresses in the Figure 2 "Memory Map" in RM0440:

So, 0x1FFF 7810 and 0x1FFF F810 will be updated to 0x1FFF 7830 and 0x1FFF F830.

Thank you for your contribution.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
TwelveSquared
Associate III
August 28, 2020

Hello @Imen DAHMEN​ 

Thank you for confirming and raising the issue internally. Looking forward to the corrected datasheet.

Thanks