Skip to main content
Alan Tan
Associate II
November 10, 2019
Question

Missing counter using TIMER input count

  • November 10, 2019
  • 4 replies
  • 1005 views

Hi all,

I'm using nucleo STM32 L4R5ZI .

Using systick 120Mhz as clock

and set timer 2 , channel 1 as TIM_TS_TI1FP1 (Trigger and rising edge)

Then, using

int count = __HAL_TIM_GetCounter(&htim2); to sample the count for every 1ms.

Input 40KHz .

By right, the count for every 1ms is 40.

Somehow, a count will miss on every 4th ms, will be 39 for 4th, 8th 12thms.

Anyone has any idea what is going wrong?

 /* USER CODE BEGIN TIM2_Init 0 */
 
 /* USER CODE END TIM2_Init 0 */
 
 TIM_SlaveConfigTypeDef sSlaveConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 /* USER CODE BEGIN TIM2_Init 1 */
 
 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = TIMER_MAX;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
 sSlaveConfig.InputTrigger = TIM_TS_TI1FP1;
 sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_RISING;
 sSlaveConfig.TriggerFilter = 15;
 if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */
 
 /* USER CODE END TIM2_Init 2 */
	int count = __HAL_TIM_GetCounter(&htim2);

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
November 10, 2019

One or both clocks (i.e. the external signal and the STM32 clock) may be unprecise. The difference is roughly 1 in 160, i.e. around 0.6%.

What is the primary clock source in STM32, MSI or HSI or HSE?

What is the 40kHz signal's source?

JW

PS. Please change your user name to a normal nick.

Alan Tan
Alan TanAuthor
Associate II
November 11, 2019

40k signal source is coming from function generator for testing.

I set to 120Mhz using PLL.

That is probably PLL clock is not accurate.

I should try from crystal oscillator

Tesla DeLorean
Guru
November 10, 2019

How good is your external clock source (HSE) or are you relying of VCO/PLL and HSI of some pretty arbitrary accuracy?

Perhaps quantify 120 MHz in TIM2 or TIM5 vs a GPS 1PPS input.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Alan Tan
Alan TanAuthor
Associate II
November 11, 2019

I'm relying on PLL.

Tim2 40Khz was coming from function generator.