Minor error on reference manual RM 0410
Hi in the reference manual for for STM32F76xxx and STM32F77xxx which can be found here:
There is a small typo on Section 2.2.2 Figure 2 that shows the Memory Map.
The error is in the Reserved Area above Flash memory on ITCM interface which should start from the end of Flash and should be 0x00400000 - 0x07FFFFFF instead of
0x0030000 -
0x0
7FFFFFF
which conflicts with the area for the ITCM Flash I/F
#reference-manual-error