Question
MicroXplorer v3.2 - GPIO Alternate Function Configuration
Posted on February 08, 2014 at 19:16
Looking at the tutorial for MicroXplorer (
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00063255.pdf
) page 32 figure 38 shows the GPIO configuration for USART pins. In the figure, the USART pins are set to either Input or Output GPIO pins. I was under the impression that they should be set to alternate function mode, ''For other peripherals: Configure the desired I/O as an alternate function in the GPIOx_MODER register'' (RM0090, Doc ID 018909 Rev 5, page 269). In MicroXplorer and in software, should USART and other peripheral pins be configured as Input/Ouput or as Alternate Function? Also, why does MicroXplorer not configure them as Alternate Function by default (assuming that is the correct configuration)? On a side-note, are there any estimates of when a new release of MicroXplorer (with peripheral configuration) will be released? #microxplorer