Skip to main content
Moritz M
Associate II
May 31, 2012
Question

MicroXplorer as Eclipse plugin with Linux

  • May 31, 2012
  • 3 replies
  • 1014 views
Posted on May 31, 2012 at 12:27

Hi,

does anybody use the MicroXplorer Eclipse plugin with Linux and Eclipse 3.7?

Here it either crashes Eclipse or I can't choose an MCU.

Moritz

#microxplorer-ubuntu64-crashes
    This topic has been closed for replies.

    3 replies

    colignya3
    Associate
    September 6, 2012
    Posted on September 06, 2012 at 23:06

    Mine also cannot operate,

    using Ubuntu 64 with Eclipse Indigo,

    the following eclipse.ini at least and at last got me opening all:

    -startup

    plugins/org.eclipse.equinox.launcher_1.2.0.v20110502.jar

    --launcher.library

    plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505

    -showsplash

    org.eclipse.platform

    -vm

    /usr/lib/jvm/java-7-oracle/jre/bin/java

    --launcher.XXMaxPermSize

    2048m

    --launcher.defaultAction

    openFile

    -vmargs

    -Xms128m

    -Xmx2048m

    All else is well.

     

    But if I stretch the MicroXplorer menu open, it crashes.

    [I pull the separation bar up so that the blue MicroXplorer icon get larger]

    Before it crashes - I also cannot select MCU's

    I tried everything I could find on the net.

    [I did install everything the proper way]

    Tired, Desperate...

    colignya3
    Associate
    September 7, 2012
    Posted on September 07, 2012 at 08:34

    System

    It is an Intel MB, 16Gig RAM, Quad Processor

    Nvidea graphics

    colignya3
    Associate
    September 7, 2012
    Posted on September 07, 2012 at 08:35

    UBUNTU error report:

    The crashed program seems to use third-party or local libraries:

    /home/za/eclipse/plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505/eclipse_1407.so

    /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-gtk-3740.so

    /home/za/eclipse/configuration/org.eclipse.osgi/bundles/84/1/.cp/os/linux/x86_64/libunixfile_1_0_0.so

    /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-atk-gtk-3740.so

    /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-pi-gtk-3740.so

    /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-cairo-gtk-3740.so

    It is highly recommended to check if the problem persists without those first.

     

    What do I do with this?