Skip to main content
dixon
Associate II
November 4, 2016
Question

Microcontroller programming issue after connecting VBUS

  • November 4, 2016
  • 1 reply
  • 624 views
Posted on November 04, 2016 at 14:19

Hey

I am using STM32F429VIT6. I have ported the USB_CDC program from the example and was working fine with the Evaluation board. I have changed the program to work with the MCU and ported the program. I havent enabled the VBUS pin. The compuuter was not detecting the USB. So the next time I enabled the VBUS and connected to the laptop using cable. Again it was not detecting. But after that I am not able  to program my MCU using serial wire using St_link. ST_link utility says the target detection failed. lease Help. How should I connect to the laptop to be detected when working as CDC 
    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    November 18, 2016
    Posted on November 18, 2016 at 15:28

    Hello,

     Make sure that you've configured the right pins and check all connections to ST-Link.

    Regards