Skip to main content
shabbir.hussain
Associate II
Jul 31, 2019 9:23 PM UTC
Solved

Memory Mapped QSPI reads nonsensical data

I am using a STM32F746zg uc connected to a W25Q80 Flash memory. In my initialization I erase a page then memory map the flash and then I read a pointer to that address. I expect to read 0xFF as the flash has just been erased, however I read 0x88. I'm not sure what is causing this behavior. Have I improperly wired the flash or is this an issue with my code (see snippets below)?

More Info:

  1. I'm using Cube IDE and created the project using Cube MX.
  2. I am able to properly read the manufacturer and device ID so I know that atleast vcc, gnd, cs, clk, io0 are wired properly.
  3. I followed the cubef7 example for memory mapped qspi as closely as possible

int EraseSector(QSPI_HandleTypeDef* hqspi, QSPI_CommandTypeDef* sCommand, QSPI_AutoPollingTypeDef* sConfig, uint32_t addr)
{
	sCommand->Instruction = SECTOR_ERASE_CMD;
	sCommand->AddressMode = QSPI_ADDRESS_1_LINE;
	sCommand->Address = addr;
	sCommand->DataMode = QSPI_DATA_NONE;
	sCommand->DummyCycles = 0;
 
 if (HAL_QSPI_Command(hqspi, sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
	 return 0;
 }
 
	/* Configure automatic polling mode to wait for memory ready ------ */
	 sCommand->InstructionMode = QSPI_INSTRUCTION_1_LINE;
	 sCommand->Instruction = READ_STATUS_REG_CMD;
	 sCommand->AddressMode = QSPI_ADDRESS_NONE;
	 sCommand->AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
	 sCommand->DataMode = QSPI_DATA_1_LINE;
	 sCommand->DummyCycles = 0;
	 sCommand->DdrMode = QSPI_DDR_MODE_DISABLE;
	 sCommand->DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
	 sCommand->SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
 
	 sConfig->Match = 0x00;
	 sConfig->Mask = 0x01;
	 sConfig->MatchMode = QSPI_MATCH_MODE_AND;
	 sConfig->StatusBytesSize = 1;
	 sConfig->Interval = 0x10;
	 sConfig->AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
 
	 if (HAL_QSPI_AutoPolling(hqspi, sCommand, sConfig, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
	 {
		 return 0;
	 }
 
	 return 1;
}
int SetMemoryMap(QSPI_HandleTypeDef* hqspi, QSPI_CommandTypeDef* sCommand)
{
	// Memory Map the External flash
	QSPI_MemoryMappedTypeDef s_mem_mapped_cfg;
 
	/* Configure the command for the read instruction */
	sCommand->InstructionMode = QSPI_INSTRUCTION_4_LINES;
	sCommand->Instruction = QUAD_OUT_FAST_READ_CMD;
	sCommand->AddressMode = QSPI_ADDRESS_4_LINES;
	sCommand->DataMode = QSPI_DATA_4_LINES;
	sCommand->DummyCycles = DUMMY_CLOCK_CYCLES_READ_QUAD;
 
 	/* Configure the memory mapped mode */
 	s_mem_mapped_cfg.TimeOutActivation = QSPI_TIMEOUT_COUNTER_DISABLE;
 	s_mem_mapped_cfg.TimeOutPeriod = 0;
 
 	if (HAL_QSPI_MemoryMapped(hqspi, sCommand, &s_mem_mapped_cfg) != HAL_OK)
 	{
 		return 0;
 	}
 
 	return 1;
}
 /* Reading Sequence ------------------------------------------------ */
	 __IO uint8_t *qspi_addr = (__IO uint8_t *)(0x90000000);
	 for (int idx = 0; idx < BUFFERSIZE; idx++)
	 {
		if (*qspi_addr != aTxBuffer[idx])
	 {
			 HAL_GPIO_TogglePin(GPIOB, LD3_Pin);
		}
		qspi_addr++;
	 }

This topic has been closed for replies.
shabbir.hussain
shabbir.hussainBest answer
Associate II
Aug 2, 2019 7:54 PM UTC

I've solved my issue thanks to @Andreas Bolsch​  and @Community member​ 

The problems were due to the fact that the flash expects a 24 bit address and I was just supplying an 8-bit address. The fix is in the command settings specified in the HAL command config to set the address size to 24 bit. The working code to map memory is pasted below in case someone stumbles upon this issue.

int SetMemoryMap(QSPI_HandleTypeDef* hqspi, QSPI_CommandTypeDef* sCommand)
{
	// Memory Map the External flash
	QSPI_MemoryMappedTypeDef s_mem_mapped_cfg;
 
	/* Configure the command for the read instruction */
	sCommand->InstructionMode = QSPI_INSTRUCTION_1_LINE;
	sCommand->Instruction = QUAD_OUT_FAST_READ_CMD;
	sCommand->AddressMode = QSPI_ADDRESS_1_LINE;
	sCommand->AddressSize		= QSPI_ADDRESS_24_BITS;
	sCommand->DataMode = QSPI_DATA_4_LINES;
	sCommand->DummyCycles = DUMMY_CLOCK_CYCLES_READ_QUAD;
 
 	/* Configure the memory mapped mode */
 	s_mem_mapped_cfg.TimeOutActivation = QSPI_TIMEOUT_COUNTER_DISABLE;
 	s_mem_mapped_cfg.TimeOutPeriod = 0;
 
 	if (HAL_QSPI_MemoryMapped(hqspi, sCommand, &s_mem_mapped_cfg) != HAL_OK)
 	{
 		return 0;
 	}
 
 	return 1;
}

8 replies

Tesla DeLorean
Guru
Aug 1, 2019 1:15 AM UTC

I think by default the part is not in Quad mode.

Try using the non-mapped Single, Double and Quad reads prior to trying mapped.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
shabbir.hussain
Associate II
Aug 1, 2019 8:42 PM UTC

I tried this. I read 0xFF which is expected after erasing the memory. My next step is to read back something I wrote in.

int ReadData(QSPI_HandleTypeDef* hqspi, QSPI_CommandTypeDef* sCommand, uint32_t addr)
{
	 uint8_t reg;
 
	 /* Read Volatile Configuration register --------------------------- */
	 sCommand->InstructionMode = QSPI_INSTRUCTION_1_LINE;
	 sCommand->Instruction = READ_CMD;
	 sCommand->AddressMode = QSPI_ADDRESS_1_LINE;
	 sCommand->Address			 = addr;
	 sCommand->DataMode = QSPI_DATA_1_LINE;
	 sCommand->DummyCycles = 0;
	 sCommand->SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
	 sCommand->NbData = 1;
 
	 if (HAL_QSPI_Command(hqspi, sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
	 {
		 return 0;
	 }
 
	 if (HAL_QSPI_Receive(hqspi, &reg, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
	 {
		 return 0;
	 }
 
 
	 return reg;
}

Andreas Bolsch
Lead III
Aug 1, 2019 7:08 AM UTC

This particular chip doesn't have a 'pure' quad mode at all. Even for the quad-I/O instructions, the instruction byte must be send in 1-line mode (in contrary to your 'sCommand->InstructionMode = QSPI_INSTRUCTION_4_LINES;' in SetMemoryMap), only address and data can be transferred in quad mode. It's a rather old design ...

Moreover, before using the quad-I/O-instructions, the non-volatile QE bit in the status register 2 must be set (in 1-line-mode, of-course) once. And watch out for the rather peculiar features of the 'Write status register' instruction for this device.

Tesla DeLorean
Guru
Aug 1, 2019 8:12 AM UTC

Even with a 1-bit instruction and address, a linear mapped read of the array can run at 66 or 100 MBps​ on a F7 running at 200 MHz

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andreas Bolsch
Lead III
Aug 2, 2019 11:24 AM UTC

Did you really check that QE was successfully set? Your SetQERegister can't work as desired: A write to status register takes up to 15 ms to complete! And, as already mentioned above, don't toggle the QE bit, just set it to '1'. This has to be done only once, as it's a non-volatile setting, so don't set it unconditionally but only when it's still '0'.

What's WRITE_ENABLE_VOL_STATUS_REG? For writing to the status register*S*, the usual WRITE_ENABLE instruction is required, nothing else.

Did you check that all GPIOs involved are set properly to AF and that the correct AF number is selected? Any activity on the IO3, IO2 pins? After setting QSPI to memory mapped mode, did you check that the QSPI registers are properly initialized? Verify in particular CR and CCR against reference manual. BUSY bit set, any errror flag in SR set?

shabbir.hussain
shabbir.hussainAuthorBest answer
Associate II
Aug 2, 2019 7:54 PM UTC

I've solved my issue thanks to @Andreas Bolsch​  and @Community member​ 

The problems were due to the fact that the flash expects a 24 bit address and I was just supplying an 8-bit address. The fix is in the command settings specified in the HAL command config to set the address size to 24 bit. The working code to map memory is pasted below in case someone stumbles upon this issue.

int SetMemoryMap(QSPI_HandleTypeDef* hqspi, QSPI_CommandTypeDef* sCommand)
{
	// Memory Map the External flash
	QSPI_MemoryMappedTypeDef s_mem_mapped_cfg;
 
	/* Configure the command for the read instruction */
	sCommand->InstructionMode = QSPI_INSTRUCTION_1_LINE;
	sCommand->Instruction = QUAD_OUT_FAST_READ_CMD;
	sCommand->AddressMode = QSPI_ADDRESS_1_LINE;
	sCommand->AddressSize		= QSPI_ADDRESS_24_BITS;
	sCommand->DataMode = QSPI_DATA_4_LINES;
	sCommand->DummyCycles = DUMMY_CLOCK_CYCLES_READ_QUAD;
 
 	/* Configure the memory mapped mode */
 	s_mem_mapped_cfg.TimeOutActivation = QSPI_TIMEOUT_COUNTER_DISABLE;
 	s_mem_mapped_cfg.TimeOutPeriod = 0;
 
 	if (HAL_QSPI_MemoryMapped(hqspi, sCommand, &s_mem_mapped_cfg) != HAL_OK)
 	{
 		return 0;
 	}
 
 	return 1;
}