Skip to main content
Associate II
November 7, 2023
Question

measure power consumption of STM32F769I-DISCO

  • November 7, 2023
  • 1 reply
  • 1605 views

i want to measure the power consumption of my stm32f769 discovery board, while its runs a simple NN model. Is there any way to do it using the STMCubeMX? or do i need to get a X-NUCLEO-LPM01A power shield? If so, would that be compatible with the STM32F769I-DISCO? @Stephanie Low @FBL 

This topic has been closed for replies.

1 reply

Jaroslav JANOS
ST Employee
November 7, 2023

Hi @aben118,

yes, you need the X-NUCLEO-LPM01A power shield, which is compatible thanks to the Arduino connector. Then, you can monitor power with STM32CubeMonitor-Power (link).

BR,
Jaroslav

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.