Skip to main content
ranran
Senior
February 26, 2019
Question

MDMA size limit of 128

  • February 26, 2019
  • 0 replies
  • 408 views

Hello,

I see that MDMA is limited to 128 bytes (BufferTransferLength).

Yet, when using DMA (with HAL_SRAM_Read_DMA for example) we can use larger size (up to 65536).

Yet, I don't see in code that DMA is triggered more than once.

Is it that these multiple transfers are done within controller and are transparent in HAL usage ?

Thanks,

ran

This topic has been closed for replies.