Question
MCU Voltage Level vs USB FS
Posted on April 23, 2013 at 07:36
Hi,
My F4 MCU is running at 2.8V, but I need to use USB OTG FS peripheral.MCU is device mode (peripheral mode) and not bus powered, I only use vbus, for detect dm-dp signals entity.Data is bidirectionalVBus, DM,DPBut, there is a threshold VIHZ
2.7V for D+ AND D- signals. (In USB 2.0 Spec, 7.1.4, Fg: 7.26)So if any of D+, D- drops under 2.7V, result: ''Device disconnected''As far as I understand I need to translate voltage levels for D+ and D-. (vbus not neccessary)Note: Solution must be low price.1. How can I do it properly? Which IC do I need to use for given specs?2. Can I connect Vbus directly to MCU?