MCU stop working suddenly (LED driven by the MCU is off), can not be programmed anymore
Hi,
I use STM32H7A3LIH6Q in my project. Now we have two prototypes and I could program and run them at the beginning, LED is on or blinking.
Later when I started to test the DC/DC converter, both boards had LED (driven by MCU) off, and can not be programmed any more.
No smoke or smell happened.
The LED suddenly got off When I probe a test point (ITH pin of DC/DC converter) on DC/DC for the first board, and when I did load test to the 3.3 V rail for the second board.
The power is ok, oscillator still works. The Vcore of the MCU is 1.3 V still, I’m wondering what could go wrong with the MCU, and since the MCU is not programmable at all, any thoughts to make it programmable again?
By the way, we use SWD, and those pins are designed for SWD.
Any response is appreciated.
Jasmine