Skip to main content
PNada.1
Associate III
January 31, 2020
Question

MCU selection

  • January 31, 2020
  • 2 replies
  • 564 views

I am looking for an MCU for a new project. Desired features:

Ethernet, EEPROM, I2C, UART, SPI, PWM, 1MB flash, USB, ETM, possibly TQFP package, no BGA, operating voltage 3 - 3.6 V, OR 5V, -40C to 85 C operating range. 

Thanks,

Priya

    This topic has been closed for replies.

    2 replies

    STOne-32
    ST Technical Moderator
    January 31, 2020
    Piranha
    Principal III
    January 31, 2020

    Doesn't exist, because EEPROM exists only in L0 and L1 series, which doesn't have Ethernet. Use external EEPROM, FRAM, software EEPROM emulation or other type of storage and look for devices with Ethernet in F1, F2, F4, F7 and H7 series.

    The most important rule - don't expect ST's provided bloatware code (HAL, CubeMX, examples) to work, especially for Ethernet and USB.

    And, talking about Ethernet, prepare for this: https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32