Skip to main content
Senior
November 17, 2023
Solved

MCU operating temperature varies between two identical board

I am currently developing the firmware for a project.  I have two boards, running identical firmware but the operating temperature between the MCUs on the boards has about a 10°C difference, 43°C vs 53°C (confirmed with a thermal camera).

We have more boards, but before I go too far with this, I was hoping to get some input from someone on what to expect.  I checked the power supply voltage on both boards and it is identical at 3.40V.

The STM32G474 is running at 144MHz with 230.4kBd continuous serial communications.  There are two DSMPS power supplies each using one HRTIM PWM signal from the MCU, switching at 200kHz.

There are 9 ADC channels being monitored continuously.  The average main loop execution time it 39us with a worst case of 83us.

Any thoughts?

 

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
November 17, 2023

i just can guess...this seem to high anyway.

your G474 should need about 25mA (144Mhz, core);

i have a H743 here, should need 53mA (200MHz, core);

i have some peripherals running , should be similar your setup.

and i get 32° (IR thermo.), at 22° ambient. so your G474 should be < 30° anyway.

there is something wrong on your boards, not only the 53° is too high, also the other.

If you feel a post has answered your question, please click on " Best Answer ".

7 replies

AScha.3
AScha.3Best answer
Super User
November 17, 2023

i just can guess...this seem to high anyway.

your G474 should need about 25mA (144Mhz, core);

i have a H743 here, should need 53mA (200MHz, core);

i have some peripherals running , should be similar your setup.

and i get 32° (IR thermo.), at 22° ambient. so your G474 should be < 30° anyway.

there is something wrong on your boards, not only the 53° is too high, also the other.

If you feel a post has answered your question, please click on " Best Answer ".
Senior
November 17, 2023

Thank you, I'll have to take a deeper look.  Maybe an I/O pin conflict.  

AScha.3
Super User
November 17, 2023

right, and check vcore - about 1,2V at the vcap caps.

i just checked a H563 , at 250MHz, is at 28,8° . (32mA at 250M,core only, this should be more similar your G474 )

If you feel a post has answered your question, please click on " Best Answer ".
LCE
Principal III
November 17, 2023

Any other loads at the GPIOs?

And check the other electronics, too.
Maybe something else on the other side of the PCB?

Senior
November 17, 2023

The most significant intended load are 3 LEDs that will draw a maximum of 6.2mA at maximum VDD.  I do have two pins that are fed by -12V through a 10k resistor than a Schottky diode to ground, so there could be some negative voltage at those pins.  From a graph in the data sheet of the Schottky, at 1.2mA of current the voltage drop is 3.3V maximum at 2mA but typically 2.2V.  The 3.3V would exceed the input voltage absolute maximum.  But luckily, I caught this issue and added series resistor between the Schottky and the MCU pin before approving the 1000 board getting fabricated.

My main concern is that the problem is different between the two boards I am working with. 

Thank you for your suggestions.

My client is testing a board and the MCU on that board is only 30°C but they are in a lab that is much cooler than my office.