Skip to main content
SKomu.1
Visitor II
February 25, 2021
Question

MCU gets stuck when enabling DMA channel to read from GPIO register on STM32F103.

  • February 25, 2021
  • 1 reply
  • 706 views

I want to read from GPIOB in regular intervals into the RAM. After 8 hours of reading blog posts, examples and trying different things I had no success. I am using STM32Cube to generate code and I am using following code to initiate transfer. So far among many other things I tried using TMR4's tmr4_up event to trigger DMA1 Channel 7, and used following call to initiate DMA transfer.

HAL_DMA_Start(&hdma_tim4_up, &GPIOB->IDR, (uint32_t *)buffer1, sizeof(buffer1));

As soon as DMA channel is enabled execution halts and MCU gets stuck on following line;

  __HAL_DMA_ENABLE(hdma);

Using same method to read from UART1 works fine when I setup DMA channel for UART with STM32Cube.

Any help will be appreciated.

Here is DMA initialization code

  __HAL_RCC_TIM4_CLK_ENABLE();

  

  /* TIM4 DMA Init */

  /* TIM4_UP Init */

  hdma_tim4_up.Instance = DMA1_Channel7;

  hdma_tim4_up.Init.Direction = DMA_PERIPH_TO_MEMORY;

  hdma_tim4_up.Init.PeriphInc = DMA_PINC_DISABLE;

  hdma_tim4_up.Init.MemInc = DMA_MINC_ENABLE;

  hdma_tim4_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

  hdma_tim4_up.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

  hdma_tim4_up.Init.Mode = DMA_NORMAL;

  hdma_tim4_up.Init.Priority = DMA_PRIORITY_LOW;

  if (HAL_DMA_Init(&hdma_tim4_up) != HAL_OK)

  {

   Error_Handler();

  }

  __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim4_up);

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
February 25, 2021

I don't use Cube, but

> HAL_DMA_Start(&hdma_tim4_up, &GPIOB->IDR, (uint32_t *)buffer1, sizeof(buffer1));

as Size probably need number of transfers, so if you transfer halfwords, then sizeof(buffer1)/2

JW