Skip to main content
aal
Visitor II
April 10, 2013
Question

MCU firmware update with USART interface for STM32F100C8

  • April 10, 2013
  • 1 reply
  • 775 views
Posted on April 10, 2013 at 08:33

I am a new bird for this MCU. My project has two part:

(1) Main program: Using the ST MCU (P/N: STM32F100C8) totransfer data in and out 

witha Bluetooth-module through USART interface and then to Android phone:

ST MCU <--> BT module <--> Android, (all communicate with each other by USART interface)

(2) Firmware update: I would like to do the firmware update function to update the main program byan Android phone which sending the update firmware to ST MCU throughBT-module by also USART interface. 

I spent quite a lot of time searching method in this forum and other websites, 

But I just cannot make sure some method like bootloader or DFU is the way I should 

keep going. I have also checked many application note e.g. AN2606, AN3155 and AN3374... but seems that I do not have enough information to figure out the picture.

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 10, 2013
    Posted on April 10, 2013 at 12:18

    Please try to keep a single thread for this.

    [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/MCU%20firmware%20update%20with%20USART%20interface%20for%20STM32F100C8&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=1]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fMCU%20firmware%20update%20with%20USART%20interface%20for%20STM32F100C8&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=1
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..