Skip to main content
Visitor II
Oct 5, 2026 5:34 PM UTC
Question

Maximum current for all peripharals enable in sleep mode for stm32U5G9

Respected Sir/ Mam,
Can you please tell me the maximum current for all peripharals enable in sleep mode for stm32U5G9, along with the dedicated settings mode.
Thankyou

1 reply

Gyessine
ST Technical Moderator
Oct 6, 2026 8:27 AM UTC

Hello ​@Mugees Nasir 
Welcome to ST Community.
Could you please provide more details about your use case? With the information provided, I cannot give a precise answer.
Which peripherals do you plan to enable? Please note that most peripherals are turned off in Sleep mode, except for low-power peripherals. Also, which memories do you need to use, and do you intend to use LDO or SMPS?
These details can significantly affect power consumption.
For now, I recommend referring to the product datasheet tables from pages 46 to 49, which may help.
Best regards,
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.