Skip to main content
stm32forum
Associate III
March 26, 2015
Question

Max input ADC below Vss F411

  • March 26, 2015
  • 1 reply
  • 533 views
Posted on March 26, 2015 at 15:01

I was wondering what the negative input can be on an ADC pin.

We have an analog signal that can be very rare -38mV for a short moment.

In the datasheet page 60 of the F411 i can only find Absolute maximum ratings: Input voltage on FT and TC pins  VSS –0.3

So it looks I'm within the marge, is that correct ?
    This topic has been closed for replies.

    1 reply

    AvaTar
    Senior III
    March 26, 2015
    Posted on March 26, 2015 at 15:59

    ...i can only find Absolute maximum ratings: Input voltage on FT and TC pins  VSS –0.3

     

    There is, at least in my F40x datasheet, and additional column ''Unit'', which says ''V''.

    That means -300mV, so -38mV is in limits.

    However, protective measures are probably advisable.

    For small and low power negative surges, a schottky diode might be sufficient.