Skip to main content
Youssouf Coulibaly
Associate II
November 9, 2017
Question

malloc issue with 4K allocation in STM32F091CC

  • November 9, 2017
  • 4 replies
  • 1158 views
Posted on November 09, 2017 at 11:14

Hi all,

I have an application when I need to reserve 4Kbytes of memory. This size is fixed during the whole life cycle of my application.

Therefore my first idea was to create a static memory allocation. But I also tried to use the malloc function to reserve 4K memory. I am using C++ and I am calling free function in my Class destructor.

But the problem I am facing is that my application rises a hard fault when i am calling other task (no operating system).

- Task 1 is for memory management function. 

- Task 2 is for UART communication.

So I have general question since that is my first time I am working on huge memory allocation is embedded device.

Is with malloc function in STM32F091 we can allocate 4kbytes of memory ?

What is about eh default heap size ? How can I explicitely increase the heap size ?

Thanks for your help.

Regards

    This topic has been closed for replies.

    4 replies

    Andrew Neil
    Super User
    November 9, 2017
    Posted on November 09, 2017 at 11:35

    my first idea was to create a static memory allocation

    So why don't you just do that?

    Is with malloc function in STM32F091 we can allocate 4kbytes of memory ?

    What is about eh default heap size ? How can I explicitely increase the heap size ?

    These have nothing specifically to do with the chip - they depend on the particular toolchain you are using.

    So - what 

    toolchain

    you are using?  Have you checked its documentation?
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    November 9, 2017
    Posted on November 09, 2017 at 11:38

    The chip has 32K RAM. So 4K is not exactly 'huge' - though not insignificant ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Youssouf Coulibaly
    Associate II
    November 9, 2017
    Posted on November 09, 2017 at 11:58

    Hello Andrew,

    Thanks for your reply.

    Yes the chip has 32K RAM and I double check in the linker script (defined addresses OK).

    Even if I use static allocation, I have the same issue.

    SCENARIO 1 : Error in execution

    static const uint16_t SECTOR_LENGTH = 4096

    //static uint8_t ptrSectorRAMSpace[SECTOR_LENGTH];     // Methode 1 static

    uint8_t* ptrSectorRAMSpace = (uint8_t*)malloc(SECTOR_LENGTH); // Methode 2 dynamic

    SCENARIO 2 : Error in excution

    static const uint16_t SECTOR_LENGTH = 3840

    //static uint8_t ptrSectorRAMSpace[SECTOR_LENGTH];     // Methode 1 static

    uint8_t* ptrSectorRAMSpace = (uint8_t*)malloc(SECTOR_LENGTH); // Methode 2 dynamic

    SCENARIO 3 : NO ERROR

    static const uint16_t SECTOR_LENGTH = 3548

    //static uint8_t ptrSectorRAMSpace[SECTOR_LENGTH];     // Methode 1 static

    uint8_t* ptrSectorRAMSpace = (uint8_t*)malloc(SECTOR_LENGTH); // Methode 2 dynamic

    TOOLCHAIN:

    I am developing under TrueStudio using arm-atollic-eabi-g++ compiler.  

    Andrew Neil
    Super User
    November 9, 2017
    Posted on November 09, 2017 at 12:04

    Youssouf Coulibaly wrote:

    Even if I use static allocation, I have the same issue. 

    So the issue is not to do with the dynamic allocation, then - is it?

    Review standard techniques for debugging a Hard Fault; eg,

    https://community.arm.com/iot/embedded/f/discussions/3257/debugging-a-cortex-m0-hard-fault

     

    https://www.embedded.com/design/mcus-processors-and-socs/4457540/Debugging-hard-faults-in-ARM-Cortex-M0-based-SoCs

     

    etc, ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.