Skip to main content
ferrario
Associate III
June 5, 2017
Question

Mailbox Message disappears

Posted on June 05, 2017 at 13:59

I am trying to implement a Modbus sever on the STM32f746 Nucleo.

- LWIP is running

- Cache is enabled

- MPU is protecting 2 areas as non cacheable, one for the ethernet descriptors, the other one for my variables

- Socket Server is running on port 80

I added the Freemodbus1.5 library files to the project and started a standard Modbus Task.

void vMBServerTask( void *arg )

{

    eMBErrorCode    xStatus; 

    portTickType    xTicks;

    pppSetAuth( PPPAUTHTYPE_NONE, NULL, NULL );   // TO DO clean code and remove this

  

    for(;;)

    {

                if(eMBTCPInit( MB_TCP_PORT_USE_DEFAULT ) != MB_ENOERR )

                {

                     printf('can't initalize modbus stack!\r\n' );

                }

                else if( eMBEnable(  ) != MB_ENOERR )

                {

                     printf('can't enable modbus stack!\r\n' );

                }

                else

                {

                    eMBEventType eEvent=EV_READY;

                    xMBPortEventPost(eEvent);   //Just a saty test

                    do

                    {                

                          /* Application code here. */

                          xStatus = eMBPoll();

                          /* Update input registers with the current system  tick. */

                          xTicks = xTaskGetTickCount(  );

                          /* Note: little endian stuff */

                          usRegInputBuf[0] = ( USHORT ) ( xTicks );

                          usRegInputBuf[1] = ( USHORT ) ( xTicks >> 16UL );

                    }

                    while( ( xStatus == MB_ENOERR )/* && ( ePPPThrCtlCur == CONNECTED ) */);

                    ( void )eMBDisable(  );

                    ( void )eMBClose(  );

                }

            }

}

Code compliles fine but in portvent.c where I needed to update the call

  xMailBox = sys_mbox_new(  );    //this call is outdated

  with

    if (sys_mbox_new( &xMailBox, 8)!=ERR_OK)

    {

        printf ('Failed to init Mailbox');

        return (FALSE);

    }

    else

    {

        printf ('Mailbox Init OK');

        return (TRUE);

    }

Modbus connection works fine.

The issue arises when sending a MODBUS request

1- The stack works fine, connection is accepted and the callback

prvxMBTCPPortReceive(...)

is called when I request data from my pc.

This funciton  in turn calls

sys_mbox_post( xMailBox, &eMailBoxEvent );

that shows no problems and returns osOK.

Now the task polls the Mailbox

uiTimeSpent = sys_arch_mbox_fetch( xMailBox, &peMailBoxEvent, MB_POLL_CYCLETIME );

returns a timeout, so no messages. The posted message apparently disappeared making my efforts nonsense.

I am working with TRUE Studio.

Hope somebody can help me..

Fabio

    This topic has been closed for replies.

    2 replies

    ferrario
    ferrarioAuthor
    Associate III
    June 5, 2017
    Posted on June 05, 2017 at 23:03

    A partial rewrite of the library, completely removing the MailBox, fixed the problem.

    Kinda brute force. Modbus requests are processed rightaway once the TCP Stack and 

    This solution has a smaller memeory footprint and runs ok @1ms. 

    Maximum latency has been measured over a couple of hours.

    If somebody is intereted mail me.

    lukasz2
    Associate III
    September 28, 2017
    Posted on September 28, 2017 at 14:14

    Hi,

    I am also trying to implement Modbus server. I have a problem with  sys_mbox_post( xMailBox, &eMailBoxEvent ); because it never ends when data is received. I am interested your solution. Can you share it?