Skip to main content
user 143
Associate III
September 25, 2017
Question

LwIP with ethernet interrupt

  • September 25, 2017
  • 7 replies
  • 4722 views
Posted on September 25, 2017 at 15:23

Hey guys,

for speed optimization I want to use ethernet interrupt when a new packet recieves. For this, first I changed heth.Init.RxMode to ETH_RXINTERRUPT_MODE and after that I added the interrupt handler with:

void HAL_ETH_RxCpltCallback(ETH_HandleTypeDef *heth)

{ }

This works so far fine. For example I can toggle a LED in the interrupt handler. 

Now I removed the ethernetif_input(&gnetif); call from the main while loop and put it into the interrupt handler. 

Well, this isn't working really fine. I recieve a few packets, but then the interrupt isn't calling anymore. 

So I searched for my mistake and had an idea. What happens when a packet is in the stack and a interrupt is calling? 

Now I changed the interrupt handler to this:

void HAL_ETH_RxCpltCallback(ETH_HandleTypeDef *heth)

{

NVIC_DisableIRQ(ETH_IRQn);

ethernetif_input(&gnetif);

NVIC_EnableIRQ(ETH_IRQn);

}

Now it's working better, but after round 20 recieved packets it took about 5 seconds between sending a packet from the pc to the call of the interrupt. And with every received packet it's getting more worse, until I receive no more packets. 

Where is my mistake? 

Thank you. 

    This topic has been closed for replies.

    7 replies

    ST Technical Moderator
    October 18, 2017
    Posted on October 18, 2017 at 17:21

    Hello

    jurij.zapusek

    ,

    Which device using ?

    Kind Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    user 143
    user 143Author
    Associate III
    October 26, 2017
    Posted on October 26, 2017 at 10:35

    Hallo 

    Imen,

    It's a STM32F107.

    And I think I know my mistake. I'm calling the hole lwIP-Stack in an interrupt routine, was isn't realy nice. I think I get a stack overflow in the controller, so that the controller isn't working any more. 

    nguen nguyen
    Associate III
    January 6, 2019

    have the same issue

    Piranha
    Principal III
    January 7, 2019

    When receive interrupt is triggered, You must read all (!!!) received packets not just one.

    P.S. Old ST examples and demos (for example STM3210C-EVAL demo firmware) are also working ridiculously slow and unstable most likely because of this bug.

    nguen nguyen
    Associate III
    January 16, 2019

    Hallo 

     How to read all (!!!) received packets ?