Skip to main content
andreatoscan9
Visitor II
March 25, 2016
Question

LwIP doesn't receive messages after a while

  • March 25, 2016
  • 2 replies
  • 819 views
Posted on March 25, 2016 at 17:06

Hallo,

I'm developing on a board based on STM32F407 and FreeRTOS, FatFS, and LwIP. The code is generated by Cube 4.13.

The problem is that during a test with a continuous ping (-f) the board doesn't receive messages after a while. Some times it is possible to have a default header interrupt due to a illegal access memory done by alloc or free mempool functions.

In my opinion it is a matter of LwIP configuration, but I don't understand exactly what.

Does someone have a similar problem?

Any idea to debug and solve it?

Thanks.   
    This topic has been closed for replies.

    2 replies

    Walid FTITI_O
    Visitor II
    March 30, 2016
    Posted on March 30, 2016 at 18:01

    Hi toscan.andrea,

    I suggest you to start from the lwIP examples under STM32cubeF4 package to compare with your project.

    Examples under this path: STM32Cube_FW_F4_V1.11.0\Projects\STM324xG_EVAL\Applications\LwIP

    For the CubeMx side, you can refer

    to the paragraph ''B.3.6 LwIP'' in the

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00104712.pdf

    .

    For more details, you can refer to

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00103685.pdf

    “Developing applications on STM32Cube with LwIP TCP/IP stack “

    that can help you in developing you application.

    -Hannibal-

    Hallo,

    I'm developing on a board based on STM32F407 and FreeRTOS, FatFS, and LwIP. The code is generated by Cube 4.13.

    The problem is that during a test with a continuous ping (-f) the board doesn't receive messages after a while. Some times it is possible to have a default header interrupt due to a illegal access memory done by alloc or free mempool functions.

    In my opinion it is a matter of LwIP configuration, but I don't understand exactly what.

    Does someone have a similar problem?

    Any idea to debug and solve it?

    Thanks.   
    AvaTar
    Senior III
    March 31, 2016
    Posted on March 31, 2016 at 08:06

    > Any idea to debug and solve it?

     

    Instrumenting your code according to your requirements. Perhaps add GPIO toggles to visualize entry/exit of relevant functions (via a scope).

    Set up a separate network segment, with one other network participant. This could be a PC with network testing software, which allows you to send defined packages at defined times/rates. Then, test your board while gradually increasing the network load. It should then be no problem to consistently trigger your problem.

    Debugging in a real-world networks with unpredictable traffic is like fishing in muddy waters.