Skip to main content
rishavnath satapathy
Associate
July 7, 2017
Question

LTFT issue.

Posted on July 07, 2017 at 04:46

Hi There,

I am using STM32F429ZI discovery board to write an UART and 

LTDC code.

I have Entesla serial to USB converter connected to the Discovery board via TTL(I am not using RS232).

Simple use case is -Display the characters entered from PC hyperterminal.

Now Individually the USART and LTDC code are working from the following git repository, but when I merge them both only USART is working. I can see only flickering on display when I am entering characters.

I am attaching the main file here. 

I am using library/code from here - 

https://github.com/MaJerle/stm32f429

 

Any suggestion guidance is welcome.

Thanks in advance.

    This topic has been closed for replies.