Skip to main content
Matthias Dübon
Associate II
Jan 4, 2018 9:10 AM UTC
Solved

LSE config failed without battery

Posted on January 04, 2018 at 10:10

Hello all,

we designed a STM32F429ZGT6 board. We're using a RTC and integrated a battery. We produced in a first batch of 50 of these boards and observed a strange behavior on 8 of these 50 boards. 

These boards are booting and behaving 'normal' when a battery is plugged in.

When we remove the battery the boards are not working any more. We tracked down the problem to the LSE clock configuration in the SystemClock_Config function If we don't configure the LSE clock the faulty boards are booting too.

We checked the external circuits and the components, everything seems fine. The problem is also not occuring when debugging the board with a debugger.

We checked the errata doc but did not find any hint. 

I also attached a screenshot of the schematic.

Any help would be very appreciated.

Matthias

#lse #battery-backup-rtc
This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jan 4, 2018 10:57 AM UTC
Posted on January 04, 2018 at 10:57

LSE is a low-power oscillator, basically a quite sensitive analog circuit. When powered from VDD, the bias conditions are different from when powered from battery.

'works when debugging' sounds like the LSE oscillator does start up but takes longer than when powered from battery; break into the loop waiting for LSERDY and single-stepping might then cover up this fact.

Try increasing the timeout.

I don' Cube so won't help with the details.

JW

8 replies

waclawek.jan
Super User
Jan 4, 2018 9:24 AM UTC
Posted on January 04, 2018 at 10:24

Show code (the offending part of it).

JW

Matthias Dübon
Associate II
Jan 4, 2018 9:36 AM UTC
Posted on January 04, 2018 at 10:36

Hello,

the error happens here:

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_ClkInitTypeDef RCC_ClkInitStruct;

RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;

/**Configure the main internal regulator output voltage

*/

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

/**Initializes the CPU, AHB and APB busses clocks

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.LSEState = RCC_LSE_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 8;

RCC_OscInitStruct.PLL.PLLN = 336;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = 7;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

If I am disabling the bold marked code

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) is true otherwise false.

waclawek.jan
waclawek.janBest answer
Super User
Jan 4, 2018 10:57 AM UTC
Posted on January 04, 2018 at 10:57

LSE is a low-power oscillator, basically a quite sensitive analog circuit. When powered from VDD, the bias conditions are different from when powered from battery.

'works when debugging' sounds like the LSE oscillator does start up but takes longer than when powered from battery; break into the loop waiting for LSERDY and single-stepping might then cover up this fact.

Try increasing the timeout.

I don' Cube so won't help with the details.

JW

Matthias Dübon
Associate II
Jan 4, 2018 11:02 AM UTC
Posted on January 04, 2018 at 11:02

We already did that and we also delayed the initial LSE configuration, no success :(

Tesla DeLorean
Guru
Jan 4, 2018 11:33 AM UTC
Posted on January 04, 2018 at 12:33

Probably one of those circumstances where you don't want to silently fail into a while (1) loop...

Problem with a lot of Cube/HAL example code is that it crawls off in a corner and dies if you get an error or abnormal situation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..