Skip to main content
Associate
Aug 13, 2026 8:39 AM UTC
Question

LSE clock not starting correctly on STM32F103

Hello everyone,

I am using STM32F103ZG MCU in a custom board for more than 7 years; 5 years ago, for shortage issues, I change the LSE oscillator from  MC-306 32.768K-E3 (CL=6pF; ESR=50k max) to 9HT10-32.768KAZY-T (CL=7pF; ESR=70k max) and I changed the external CL capacitance from 3.3pF to 10pF. I had no problems for 5 years. Now, in several boards, the LSE clock takes long time to start or even does not start until I “perturb the system” touching the capacitors or the uC’s pins with my finger.

Looking at the uC’s datasheets it seems that the feedback resistor of the oscillator’s internal circuitry (don’t know if is a “real” resistor or an equivalent resistance given by the internal circuitry) is 5M but, with indirect measurement, it seems to be much more than 5M (like hundred times more). This is for both the old boards and the “faulty” new ones, so is not (perhaps) an issue caused by the productive process of the uC.

As I written before some faulty boards in which the LSE at last starts may or may not start again once the uC is powered off and the backup battery is not supplying the backup circuitry, so the issue is not repeatable.

Using an external 10M resistor between LSE OSC_IN and OSC_OUT pins could fix the problem so it could be a solution. What I want is to understand the problem so I want to know if the 9HT10-32.768KAZY-T values are “border line” for the F103 uC (and a slight variation in the last lot of production of the oscillator raise the LSE startup issue), what really is or how is working the 5M feedback resistor or, in general, what may cause this issue.

Thanks for your time.

Francesco

11 replies

AScha.3
Super User
Aug 13, 2026 9:01 AM UTC

Hi,

>external 10M resistor between LSE OSC_IN and OSC_OUT pins could fix the problem

Did you check on not working LSE ?  + 10M , then good working ? 

If you feel a post has answered your question, please click on " Best Answer ".
Peter BENSCH
ST Technical Moderator
Aug 13, 2026 9:12 AM UTC

Welcome ​@FrancescoV, to the community!

a small note: you forgot to also specify the respective value of the shunt capacitance C0 for the data. However, as the datasheets are currently available online, I was able to determine them, and the complete values for recalculation are:

  • MC-306 32.768K-E3
    • ESR=50k max
    • CL=6pF
    • C0=0.95pF
  • 9HT10-32.768KAZY-T
    • ESR=70k max
    • CL=7pF
    • C0=1pF  

gmargin is therefore 12.387 for the MMC-306, which is more than sufficient, but only 6.582 for the 9HT10, which is only slightly greater than the minimum of 5.

It could now be that e.g. your layout is not quite optimally designed, which was probably compensated for by the significantly larger gain margin, but is now leading to the observed problems.

Unfortunately, unlike the newer STM32 devices, the STM32F103 does not yet have an LSE with adjustable drive strength, so your only options are to check the layout and/or use a crystal with an ESR of less than 60k, ideally less than 50k. However, make sure that C0 does not become significantly greater than 1pF, because that would worsen the gain margin again.

You’re welcome to insert a picture of the layout section around the crystal here, and then we can check it together. Alternatively, take a look at the Knowledge Base article:

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Aug 13, 2026 12:47 PM UTC

Hello ​@Peter BENSCH,

thanks for your reply.

I have done those calculations but I cannot figure out if gmargin=12 was sufficient or not.

I read the paragraph “2.2.6 LSE startup in harsh environments” int he ST errata ES0346 which stands that “It is recommended to mount an additional parallel feedback resistor (from 16 MΩ to 22 MΩ) on board to help the oscillation startup in all cases”: my doubt is if the gmargin consideration is sufficient to guarantee the LSE to function correctly.

I have done some tests to figure out if the greater ESR of the 9HT10-32.768KAZY-T could be the main actor in this issue; I add a resistor between the crystal and the capacitor on the OSC_OUT side to (try to) simulate a grater crystal ESR. The value of the resistance is 56k, so 75% greater than the “true” ESR. The LSE seems to start correctly every time i power up the MCU so, or this is not a (mainly) ESR issue or this is not the right way to simulate a larger crystal’s ESR. Do You have some hint?

Thank You again

Regards

Francesco

Associate
Aug 13, 2026 2:10 PM UTC

The LSE seems to start correctly every time i power up the MCU so, or this is not a (mainly) ESR issue or this is not the right way to simulate a larger crystal’s ESR.

In the paragraph 3.8 of the AN2768 I found that this is definitely not the way to simulate a greater ESR of the crystal but is the way to estimate it’s negative resistance.

Peter BENSCH
ST Technical Moderator
Aug 14, 2026 2:22 PM UTC

The ES0336 is more related to start-up problems under the special environmental conditions mentioned. However, it can do no harm to connect such a parallel resistor. I do, however, suspect that this will not make any difference in your case.

A series resistor for the crystal, i.e. the way you have inserted it between crystal and CL, only very roughly imitates a higher ESR, because the resistor not only increases the losses of the crystal, but also changes the start-up behaviour, affects the oscillator amplitude, shifts the load on the inverter/amplifier, and can also alter the frequency. It is always important to bear in mind that ESR appears only as one partial parameter in the equivalent circuit. You should not try to force the current crystal, with its somewhat high ESR (on an STM32F103), to oscillate at all costs, but rather focus on a different crystal with the recommended parameters.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STOne-32
ST Technical Moderator
Aug 14, 2026 9:25 PM UTC

Dear ​@FrancescoV , all,

Interesting discussion. My comments are :

 

  1. can you explain what means do not start at all ?  I have seen in many designs that software loop of timeout is set for example to 2 or 5 seconds and if removed the LSE will start but with a long start-up  - more than usual.
  2. why changing directly the CL1=CL2 from 3.3pF to 10pF … I do not see a rationale in your design . I would expect only 5.3pF or 5.6pF not more to keep same equivalent loop as your working PCB . May I missed something ?  Theory says - your Cs = 12-3.3pF = 8,7pF so 14pF -8,7pF = 5,3pF
  3. The errata is only present on our STM32F103 XL density devices and was written by me :-) many years ago . We have  a weakness on that LSE design due to die size creating a leakage in OSC32_IN that is impacting the start-up condition at Cold in particular and or with water droplets or Frost. Adding that parallel high resistance will help to compensate the leakage path and will relax a bit the oscillation margin.

hope it helps and let me know your feedbacks.

Regards,

STOne-32

Associate
Aug 17, 2026 3:19 PM UTC

Hello ​@STOne-32 ,

  1. the MCU’s fw does not implements a timeout so it hang until the LSERDY is set. I could see that the clock could take minutes to start or the it not start even if I perturb the loop with the fingers.
  2. At the moment I do not remember the rationale behind this choice, maybe I considered a lower stray capacitance or I saw that, according to the datasheet, 5pF should be the lowest admittable capacitance.

If you don’t mind I desire to ask you a question: I just saw a post here in the community (

) where a user had some doubt in using 20pF capacitance with a 7pF crystal and a part of your answer was: ”using 20pF will work if GM is satisfied in nominal condition as a crystal ESR is always typical and our formula is based on ESR Max computation”. I understand that a sufficently high Gainmargin could “compensate” higher CL1-CL2 capacitors, am I right or maybe I misunderstand this part of the answer? 

Thank You

Kind Regards

Francesco

STOne-32
ST Technical Moderator
Aug 17, 2026 6:28 PM UTC

Dear ​@FrancescoV ,

Let’s assume in real design Cs=3pF (stray capacitance) including all - PCB and pin. 

Having a CL1=CL2=20pF regardless of CL value of the crystal. 

The MCU LSE is seeing an equivalent CL of  “10pF+3pF”   = 13pF   instead of 7pF as example

So what happens ?  the Crystal will try to oscillate at a slower value (negative versus Nominal value 32.768KHz)

and so the oscillation margin should be computed with a CL of 13pF instead of 7pF.   in many cases it may work as ESR typical is much lower than ESR max ( worst case provided by our crystal partners).  But we are in a gray zone and not safe.

Let me know if you have a further follow-up, Here is also a Technical Note from ECS  https://ecsxtal.com/considerations-when-designing-crystals-into-stm32-microcontrollers/

Regards

STOne-32