Skip to main content
Visitor II
Aug 13, 2025 7:07 PM UTC
Question

LPBAM in Stop 0 and Stop 1 - STM32U5

In application note AN5652, page 7 states that LPBAM can be used in Stop 0, Stop 1, and Stop 2 modes. On page 10, the peripherals that support autonomous mode are listed. Since I cannot use SPI3, I also cannot use Stop 2.

Can I configure my MCU in STM32CubeIDE (IOC file) to use LPBAM in Stop 1 mode with SPI1 or SPI2? Are there application examples for this? I have only found projects using Stop 2, and the IDE seems to list only the peripherals available for Stop 2.

This topic has been closed for replies.

1 reply

ST Employee
Aug 22, 2025 8:24 AM UTC

Hey @leo8, 

In Stop 0 and Stop 1 modes, the autonomous peripherals are: 

ADC4, DAC1, LPTIMx (x = 1 to 4), USARTx (x = 1 to 6), LPUART1, SPIx (x = 1 to 3), I2Cx (x = 1 to 6), MDF1,
ADF1, GPDMA1 and LPDMA1

However, SPI1, SPI2 are autonomous only with GPDMA1 and SRAM1 to SRAM6.

And SPI3 is autonomous only with LPDMA1 and SRAM4. 

Hope that helps! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.