Skip to main content
Jin ho An
Associate II
Jan 31, 2018 8:04 AM UTC
Solved

LoRa, Large Packet

Posted on January 31, 2018 at 09:04

HI.

I am testing with ST Discovery LoRa Kit, PingPong.

There is no problem sending / receiving 64 bytes.

However, the size of 64 bytes or more can not be transmitted or received.

Semtech says that 128 bytes are possible, but why not?
    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Jan 31, 2018 6:40 PM UTC
    Posted on January 31, 2018 at 18:40

    I think the issue as observed here is the rejection of large packets where the receiver could be distracted from reception by large corrupt packets. The size is in the header burst as I recall.

    The use case for the radio could be small control channel packets, where the radio only keys on these packets and the micro stays in deep sleep states ignoring larger bulk packets not destine for it.

    The radio software in the LRWAN explicitly configures the default max to 64 bytes, although this may be changed later programmatically.

        { MODEM_LORA, REG_LR_PAYLOADMAXLENGTH, 0x40 }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    5 replies

    Tesla DeLorean
    Guru
    Jan 31, 2018 9:57 AM UTC
    Posted on January 31, 2018 at 10:57

    The max is closer to 255 bytes. You are likely sending just fine, there is a setting on the receiving side to reject packets beyond a certain size.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    Jan 31, 2018 4:42 PM UTC
    Posted on January 31, 2018 at 17:42

    Note that the maximum size of packet depends on the the data rate you're using; eg, 

    for the European 863-870MHz band, the

    application

    packet size varies between 51 bytes for the slowest data rate, and 222 bytes for faster rates.
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Jan 31, 2018 6:40 PM UTC
    Posted on January 31, 2018 at 18:40

    I think the issue as observed here is the rejection of large packets where the receiver could be distracted from reception by large corrupt packets. The size is in the header burst as I recall.

    The use case for the radio could be small control channel packets, where the radio only keys on these packets and the micro stays in deep sleep states ignoring larger bulk packets not destine for it.

    The radio software in the LRWAN explicitly configures the default max to 64 bytes, although this may be changed later programmatically.

        { MODEM_LORA, REG_LR_PAYLOADMAXLENGTH, 0x40 }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Jin ho An
    Jin ho AnAuthor
    Associate II
    Feb 1, 2018 10:02 AM UTC
    Posted on February 01, 2018 at 10:02

     Hi Clive One

    Thank you for your reply.

    I have modified the REG_LR_PAYLOADMAXLENGTH value and it seems to be receiving to some extent. If it is set to 0x80 (128) byte, it will be received only up to about 115 bytes.

    If 0x100 (256) byte is set, no reception is possible.

    I need to know only this information.