Skip to main content
Associate II
Sep 26, 2023 4:25 AM UTC
Question

LoRa example for STM32WL | un able to read from UART

I am currently working on the LoRaWAN_END_NODE example project for a stm32WL . And I want to receive external data via uart and use the LoRaWan process continually, however I am getting problems. The UART is giving invalid data after the sequencer is being initialized.

Edit: I have tried the suggestions below, I have put the gps into a task for the sequencer to run. I have also disabled low power mode. I still get invalid data from the UART that I don't receive when the sequencer is not on.

Is this a clock issue? Any ideas?

6 replies

Issamos
Super User
Sep 26, 2023 4:47 AM UTC

Hello @STMGuitartune68 

I suggest you to integrate the UART communication in the LoRaWAN  application. That's because when you are in the while loop, the sequencer in the LoRaWAN app is activated. So, it may cause a problem integrating other APIs in the process.

Best regards.

II

Danish1
Lead III
Sep 26, 2023 8:11 AM UTC

The LoRa examples are optimised for extremely low power operation.

By default, stm32_seq.c puts the stm32 into deep sleep (with all oscillators apart from LSE stopped) except when there is LoRa activity. And under those circumstances, UARTs can't work.

Have a look for #defines like LOW_POWER_DISABLE . You would need that to be 1

Associate II
Sep 28, 2023 6:40 PM UTC

I had tried this, however no luck. The problem arrises when the RTC timers are initialized for lora. the example changes some things for hal get tick and hal inittick. Im having problems with adding to those so that the uart is on a proper clock. Any ideas?

Visitor II
Apr 29, 2024 6:46 AM UTC

Hi, I have met the same problem. Have you solved the issue so far?  I want to transfer the gps data via usart to lorawan network, but I don't know how to do that. Do you have any advices? 

Visitor II
Sep 6, 2024 3:09 PM UTC

Hello, I have the same problem me too, do you solved the issue?

Xynium
Associate III
Mar 25, 2026 4:19 PM UTC

Hi,

May be a little late ...

In    sys_conf.h

for me line 78

#define LOW_POWER_DISABLE 1

was 0.

And the UART does not lose its init in the sequencer.

Hopethishelp.

Regard

JP