Skip to main content
meghasb
Associate III
July 5, 2023
Question

Looking for the more on security documentation for Tamper implementation

Hi everyone,

Can someone pls help on this, for our project we are implementing the Tamper(STM32U585 board), we want to know more about the tamper how can we implement with the different approach, so we are looking for the more detailed documents on the tamper, if u could help me on the any documents or any process or source where we connect to get these documents for our project. If someone could help us on this would be a great help. 

This topic has been closed for replies.

5 replies

Danish1
Lead III
July 5, 2023

What documents have you looked at so far?

I would expect it to be detailed in the Reference Manual for your stm32.

Typically stm32 tamper is a low-power way of sensing when a pin state changes. Your external circuitry needs to detect when tampering occurs (e.g. opening the box - perhaps by way of a microswitch, or powering-up after removal of a screening-can - the can shorts the pin to ground).

In the event of tamper, the stm32 can clear a specific block of memory and/or record the time the tamper-event took place. This can happen even when the stm32 is in very-low-power modes such as sleep or stop. But some power must still be present - perhaps from a back-up battery, supercapacitor or coin cell.

It's then up to your main code (when normal power is restored if necessary) to check if tamper happened and do whatever you feel appropriate. This might be as simple as refusing to work until a special password is entered, or you might choose to erase the FLASH and brick the device.

meghasb
meghasbAuthor
Associate III
July 6, 2023

Thanku @Danish1 . it was helpful. but i need more detailed info, as I'm already referring the reference maula for the same.

ST Technical Moderator
July 6, 2023

Hello @meghasb ,

I advise you to have a look at this AN4759 which explains Tamper management.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
meghasb
meghasbAuthor
Associate III
July 6, 2023

Thanku @Imen.D , ill go through it.