Skip to main content
KAjay.1
Associate
April 14, 2023
Question

Looking for STM32 MCUs to meet our existing one.

  • April 14, 2023
  • 5 replies
  • 1253 views

Hi,

Looking for STM32 MCU in place of Microchip Controller ATSAM4S8BB-UUR.

Please suggest a suitable Controller.

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    April 14, 2023

    120 MHz CM4 512KB FLASH 64-WLCSP

    Nothing pin-for-pin / ball-for-ball

    Should be some in the STM32L4(+) series with similar specs

    The new STM32H5 might be worth a look. Also G0 or C0 depending on actual needs

    Any specific features/function your current design uses? USART, I2C, counts, etc.

    Floating Point Math?

    RAM/FLASH utilization?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    April 14, 2023

    Low cost focus: STM32C0/STM32G0 (F0 upgrade)

    Mainstream:general purpose STM32H5 (F4 upgrade)

    Low power focus : STM32U5 (L4/L5 upgrade)

    High Performance focus : STM32H7 (F7 upgrade)

    There should be an STM32 Finder tool either on Android or PC to narrow down the choices depending on the memory footprint and specific peripherals. WLCSP is hardly for everyone. Form factor/high volume focus ?

    Billy OWEN
    ST Employee
    April 14, 2023

    Hi @KAjay.1​,

    The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

    Regards,

    Billy

    KAjay.1
    KAjay.1Author
    Associate
    April 17, 2023

    Hi,

    Requirement is as below:

    Core Processor - ARM® Cortex®-M4

    Core Size - 32-Bit Single-Core,

    Speed - 120MHz,

    Program Memory Size -512KB (512K x 8),

    Program Memory Type - FLASHRAM Size - 128K x 8,

    Voltage - Supply (Vcc/Vdd) - 1.62V ~ 3.6V,

    Data Converters - A/D 11x12b; D/A 2x12b,

    Operating Temperature - -40°C ~ 85°C (TA)

    Peripherals : UART - 1or2, I2C -2, SPI - 1or2, USB-1

    Ozone
    Principal
    April 17, 2023

    These are just MCU parameters.

    • temperature range required by your application (industry/automotive) ?
    • code size used, RAM size used ?
    • peripherals used / required ?
    • performance load ?