Skip to main content
elharrar
Associate III
Feb 3, 2012 8:20 AM UTC
Question

Looking for SDIO+eMMC (not SD) example

Posted on February 03, 2012 at 09:20

Hi ,

I'm looking for an example with SDIO+eMMC (and not SD). Is there something like that ?

Another thing: Someone has information on eMMC commands ?

Thanks

Mikael

#google #sdio+emmc-example
This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
Feb 3, 2012 12:49 PM UTC
Posted on February 03, 2012 at 13:49

Another thing: Someone has information on eMMC commands ?

What, something like this first hit on Google?

http://rere.qmqm.pl/~mirq/JESD84-A44.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
aqueisser
Associate III
Feb 3, 2012 4:35 PM UTC
Posted on February 03, 2012 at 17:35

I've got eMMC working with the STM32 in 8 bit mode with single data rate. The STM32 SDIO peripheral doesn't support dual-edge clocking so there's no dual data rate. I don't have any of the secure features and I don't use streaming, just init, read/write single block and read/write multiple blocks. 

What information are you looking for in particular? I probably can't share all my code but I'd be glad to point you in the right direction.

Andrew

elharrar
elharrarAuthor
Associate III
Feb 4, 2012 5:09 PM UTC
Posted on February 04, 2012 at 18:09

Hi Andrew,

It is exactly what I need , an example. Please could you share your code at elharrar@hotmail.com

Thank you very very much ... 

Mikael

aoleon
Associate II
Apr 17, 2013 1:21 PM UTC
Posted on April 17, 2013 at 15:21

Hello,

I am working with a STM32f205 and a THGBM4G4D1 eMMC. I use the SDIO + DMA.

 I started from the example code from ST and used the JEDEC standard. 

I have the initialisation and erase functions working but I can't get Read and Write (single and multiple block) working. Can you please send me your low level functions at 

pmc696 _at_ hotmail _dot_ com ? 

Thanks,

Alex

vilesovds
Visitor II
Jun 24, 2014 6:27 AM UTC
Posted on June 24, 2014 at 08:27

I've got eMMC working with the STM32 in 8 bit mode with single data rate. 

Andre, please share your code of MMC driver for me vilesovds @ gmail.com. Thank you

ericofkholmdverg
Visitor II
Jul 31, 2014 6:38 AM UTC
Posted on July 31, 2014 at 08:38

Hello Andre! please share your code of MMC driver ericofkholmdverg @ gmail.com. Thanks in advance.

vukasheen
Associate
Sep 29, 2014 8:41 AM UTC
Posted on September 29, 2014 at 10:41

Hi Andrew,

Can you please share yours example with me.

vukasheen_at_gmail_dot_com

Thanks in advance.

vneff
Associate III
Mar 31, 2015 3:20 PM UTC
Posted on March 31, 2015 at 17:20

Hello Andrew,

I sorry to bother you, but if could share your code or pointers about interfacing the STM32F2 and eMMC with me it would be a great help.

I have used the STM32F2xx to access SD cards via SDIO and SPI, so I think I just need to know the differences between SDIO and eMMC access.

My email: vneff at partechgss dot com

Thanks again if you can provide me some guidance!

Vance

manuel23
Visitor II
Jun 15, 2015 11:14 AM UTC
Posted on June 15, 2015 at 13:14

hi andrew.

Show all, I would help a lot if you can share your code of eMMC driver.

this is my email yete666@hotmail.com

thank you very much for your time

Tesla DeLorean
Guru
Jun 15, 2015 11:39 AM UTC
Posted on June 15, 2015 at 13:39

3+ year old thread, if you get no response try contacting poster directly.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..