Skip to main content
Visitor II
September 25, 2024
Question

Looking For External Memory Benchmark on STM32F469/79 using FMC or QSPI interface

Hi,

Anyone know where I can find memory benchmarks on using the different type of external memories on the STM32F469/79 ?

How slower is the PSRAM on FMC or dual Quad SPI compare to internal SRAM ?

thanks

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 25, 2024

Wouldn't you just test it?

The F4 is an uncached architecture, so external interfaces are going to slam access speed.

SDRAM was 6x slow than internal SRAM, as I recall.

I haven't tried QSPI NOR Flash, but would hazard between 2 and 4x slower than Internal FLASH. That I could read Dual-Quad QPI at approaching 90 MBps in a continuous / large-linear sense, doing nothing else, perhaps loading executable code into Internal SRAM in some mapped/banked scheme.

Some pressing reason not to be using a CM7 device in 2024?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..