Looking at getting 1st STM32...
My main goto board ATM has been an Arduino Due as it has heaps of pins, 3.3v, 32 bit , 96K or SRAM, 512K of flash and easy to program straight from Visual Studio.
One thing I hate about it is all they all seem to ship with female header pins and the layout is bad.
Well, given the way things have progressed a STM32F4Discovery STM32F407VGT6 ARM Cortex-M4 really got my attention.
I have checked and have the ability to compile for it under my environment.
The specifications are ~double of my Due (CPU Mhz, flash and sram) and on top of that it mentions having a FPU.
The pin layout looks great and the price is just a tad over AUS$10 on Aliexpress.
Main thing I need is fast I/O and fast SPI with access to DMA and or FIFO.
I suppose the main question is... are there any other boards with higher specifications I'd be better jumping too?
256K SRAM would be great and I did notice some sport the ability to add more SRAM on the back.
As it is... this AU$10ish board makes all my Due's and dare I say Teeny's not worth mucking around with (not to mention the 3 Uno's I have).
I have a fast graphics library I've been developing and they get a bit hungry for SRAM and CPU cycles.